Member and Staff Blogs What's new in fairy tech?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 16 Nov 2023 1:35 AM Date Created
  • Views 2609 views
  • Likes 11 likes
  • Comments 19 comments
Related
Recommended

What's new in fairy tech?

scottiebabe
scottiebabe
16 Nov 2023

The first set of fairy lights I purchased a few years ago had a very rudimentary embodiment. Just two AA batteries, an on/off switch, and a string of miniature LEDs on enamel wire.

image

I love the simplicity of the design... The design works well enough with disposable alkaline batteries. However recharge cells don't work very well on their own, as their combided state of charge voltage very quickly drops below the forward voltage of the white LEDs.

Fairy Tech 2.0

Browsing at the dollar store today, I found some new fairy lights which included some circuitry on a PCB. What could it be?

image image

Same general look and feel as before.

image

Now included is a three position switch!

image

The mysterious PCB

image

No sign of an inductor anywhere Disappointed. Just a

- 8-pin MCU?

- Watch crystal

- SPDT Slide switch

image

Fairy Tech 3.0

I can upgrade this new set of fairy lights with a boost converter module capable of operating of a single alkaline/Ni-MH cell

image

Module based on ME2188 https://file.elecfans.com/web2/M00/64/78/poYBAGMHOg-APsG0AAge4TQOpd0961.pdf 

I bought a value pack awhile back thinking I would receive a selection of different output voltages. Nope, I got a bag of identical modules and each has a nominal output voltage of 5V. So, I added an additional 50 Ohm series resistor to limit the current to approximately 40 mA.

image

I am taking a bit of a gamble assuming the MCU is 5V rated. If it gives up the ghost, I'll replace it too.

image

All for now.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe +1
    Out of the box they can also sometimes be a bit too bright for fast lenses with wide open apertures. Arducam do a low-cost F1.6 C-Mount lens which can be used with the likes of a R-Pi HQ camera for bokeh…
  • scottiebabe
    scottiebabe over 2 years ago in reply to beacon_dave

    Splurge and take a few home.

    Musical score Walking in an RF wonderland ....

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe

    Looks like silver glitter and mirror ornaments are the in thing this year judging by the supermarket displays. Just need to distract the security staff for long enough to turn the seasonal aisle into a bokeh studio Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe

    Yes, they would be interesting to photograph.

    What I had in mind was something similar to this sort of branch-like framework structure

    imageimage

    (images from a Vectorworks 3D modelling CAD tutorial by Luis M Ruiz)

    On the left would be more like the real-life design with the pea-sized LEDs at the end of the branches (pretend the larger circle outlines aren't there) but then when you took the bokeh photograph, the light from the LEDs would then de-focus into the larger soft circles as seen on the right in the final render.

    Being able to sculpt the framework would give control over the shape and distribution of the bokeh effect in the photograph.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to beacon_dave

    I have seen a few light-up bare tree that look pretty jazzy

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe

    Perhaps using an infinity mirror or a fibre optic lamp as the background light source could produce an interesting result.

    In the past I've pondered about skeleton tree/leaf type structures with LEDs inserted at the ends so that in real life they aren't overwhelming but when you take the bokeh photograph it suddenly pops out at you.

    I'm not sure the best material to use however. I was thinking of perhaps microbore copper plumbing pipe ranging from 4-10mm outside diameter but not sure that you get Ts or reducing Ts at those sort of diameters. Also got to make it possible to thread a wire through it to the LED.

    I think it might call for a a micro brazing torch and a lot of patience.

    LED-wise then perhaps something similar to the dLUX-dLITE shaped LEDs to diffuse the light.

     https://www.adafruit.com/search?q=dLUX-dLITE

     I've seen skeleton lamps done with 1/2" plastic pipe and 40W golf ball lamps but was envisioning something a bit more intricate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>