Member and Staff Blogs What was your last Aluminum based Project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 1 Apr 2026 9:14 AM Date Created
  • Views 610 views
  • Likes 12 likes
  • Comments 11 comments
  • aluminium
  • april fools 2026
  • element13
  • gosh I love aluminium
  • aluminum
Related
Recommended

What was your last Aluminum based Project?

e14phil
e14phil
1 Apr 2026

image

element13 Certified

element13 Certified
Joined the group of element13 insiders for the metallic redesign in 2026!

What was your last Aluminum Based Project?

To celebrate our change to element13, we want to know your proudest aluminium  based projects or moments of victory! 

Was it making our favorite metal from dirt?
image
Source: https://maurycyz.com/projects/al/ 

Was it using Aluminum electrolytic capacitors?

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Or maybe a (Classic) Can Crusher? 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Tell us about your favorite project using our favorite element13.

 

  • Sign in to reply

Top Comments

  • dougw
    dougw 6 months ago +2
    Here are a couple of projects that might qualify... Thread Tapping Test StirlingEngine
  • genebren
    genebren 6 months ago +1
    I have been working on a path lighting design for a while now. I have recently completed the project and I have some pictures. The path lights are based on Pittsburgh Corning Architectural Glass Blocks…
  • DAB
    DAB 6 months ago +1
    The last time I used aluminum was to make an electrostatic detector. I used an old soda bottle, a length of copper wire with a hook at the end with two aluminum strips at the end. When the electric…
  • obones
    obones 6 months ago

    I know I'm late to the party, but here are pictures of my aluminium based project:

    image image

    The basic idea was to "channel" the RF waves for this human movement detector so that it would detect only movement coming at it from the forward direction.

    Worked well on the bench, now  I have to install it beneath the stairs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 6 months ago

    The last time I used aluminum was to make an electrostatic detector.

    I used an old soda bottle, a length of copper wire with a hook at the end with two aluminum strips at the end.

    When the electric charge accumulated, the two strips would slowly push apart to indicate the electrostatic charge in the air.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • h-elsner
    h-elsner 6 months ago

    I made a mount for a thermal imaging camera (formerly used by a drone) using wasted aluminium parts. The aim was to use the camera on a tripod to give it a second life.

    I have no 3D printer. That's why I often use other material like aluminium or wood. The camera mount can be disassembled for space-saving transport.

    yuneecpilots.com/.../

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren 6 months ago

    I have been working on a path lighting design for a while now.  I have recently completed the project and I have some pictures.  The path lights are based on Pittsburgh Corning Architectural Glass Blocks (modified with a rectangular opening on one side).  I needed to fabricate a plate that could hold the blocks (using the rectangular opening on the bottom face) and allow for a secure mounting to some 1/2" EMT conduit (5V power inlet).  I choose to use aluminum (with a small amount of steel) to build the base plates.

    Here is one of the finished blocks:

    image

    The center mounted 1/2" Compression EMT Connector is mounted into a hex cutout in a plate that is attached to the base plate (preventing the EMT connector from spinning while tightening the compression nut).  Along either side of the connector are slots (and mounting screws) that are used to provide a pair of sliding bars that secure the glass block by sandwiching the glass between the steel bar and the aluminum base plate.

    image 

    The sliding bars are held into position with a pair of aluminum channel pieces.  Between the steel bars and the base of the channel is a piece of UHDP to allow the bars to smoothly slide through the channel.

    image

    The steel bars have aluminum thread-serts (6/32 threads) allow the bars to be tightened down with sufficient force to trap the glass block to the base plate (once the bars are extended to overlap the edge of the glass block).  Weather stripping is used to produce a mostly watertight seal.

    This design went through multiple interactions during the development process.  These images are taken from the from the first workable prototype and are very rough, but still serviceable parts.  I had originally planned to use 3D printed slider blocks (I even tried some machined parts out of UHDP), but these parts distorted under the pressure of tightening, hence the change to aluminum.

    image

    It was fun to shift from silicon to aluminum for a while (except for the splinters and dulling drill bits).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw 6 months ago

    Here are a couple of projects that might qualify...

    imageThread Tapping Test

    imageStirlingEngine

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>