Member and Staff Blogs Wio Terminal - Battery Fuel Gauge
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 8 Jan 2021 4:49 AM Date Created
  • Views 6000 views
  • Likes 5 likes
  • Comments 8 comments
  • battery fuel gauge
  • ti bq27441
  • wio terminal
Related
Recommended

Wio Terminal - Battery Fuel Gauge

ralphjy
ralphjy
8 Jan 2021

The new version of the Battery Chassis add-on for the Wio Terminal has added an On-Off button and a Texas Instrument's BQ27441 Battery Fuel Gauge https://wiki.seeedstudio.com/Wio-Terminal-Chassis-Battery(650mAh)/  .

 

The fuel gauge is a great feature that measures your battery's voltage to estimate its charge percentage and remaining capacity. The chip is also hooked up to a current-sensing resistor, which allows it to measure current and power.  The fuel gauge interfaces using I2C.  This will be useful to monitor the battery in remote datalogging applications.

 

TI BQ27441

image

 

image

There is a SparkFun Arduino library https://github.com/sparkfun/SparkFun_BQ27441_Arduino_Library  .  The library abstracts away all of the low-level I2C communication, so you can easily initialize the fuel gauge then read voltage, state-of-charge, current, power, and capacity. It also implements all of the chip's low-battery, and SoC-change alerts on the GPOUT pin.

 

Here is a demo of Battery Status display on the Wio Terminal during discharging (running on battery power) and charging (running and charging from USB).  I haven't quite figured out "State of Health" yet - it always returns 0%.  And I'm not sure why the full battery capacity is incorrect (it should be 650 mAh).  I'll need to read through the BQ27441 spec.  And I also haven't been able to get the correct schematic for the new Battery Chassis, but I've requested it on the SEEED forum.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Wio_Terminal_Battery_Gauge.ino

#include <SparkFunBQ27441.h>
#include"TFT_eSPI.h"

TFT_eSPI tft;
TFT_eSprite spr = TFT_eSprite(&tft);  // Sprite
#define FF17 &FreeSans9pt7b

const unsigned int BATTERY_CAPACITY = 650; // Set Wio Terminal Battery's Capacity 

void setupBQ27441(void)
{
  // Use lipo.begin() to initialize the BQ27441-G1A and confirm that it's
  // connected and communicating.
  if (!lipo.begin()) // begin() will return true if communication is successful
  {
  // If communication fails, print an error message and loop forever.
    Serial.println("Error: Unable to communicate with BQ27441.");
    Serial.println("  Check wiring and try again.");
    Serial.println("  (Battery must be plugged into Battery Babysitter!)");
    tft.setTextColor(TFT_RED);
    tft.setCursor((320 - tft.textWidth("Battery Not Initialised!"))/2, 120);
    tft.print("Battery Not Initialised!");
    while (1) ;
  }
  Serial.println("Connected to BQ27441!");

  // Uset lipo.setCapacity(BATTERY_CAPACITY) to set the design capacity
  // of your battery.
  lipo.setCapacity(BATTERY_CAPACITY);
}

void printBatteryStats()
{
  // Read battery stats from the BQ27441-G1A
  unsigned int soc = lipo.soc();  // Read state-of-charge (%)
  unsigned int volts = lipo.voltage(); // Read battery voltage (mV)
  int current = lipo.current(AVG); // Read average current (mA)
  unsigned int fullCapacity = lipo.capacity(FULL); // Read full capacity (mAh)
  unsigned int capacity = lipo.capacity(REMAIN); // Read remaining capacity (mAh)
  int power = lipo.power(); // Read average power draw (mW)
  int health = lipo.soh(); // Read state-of-health (%)

  // Now print out those values:
  String toPrint = String(soc) + "% | ";
  toPrint += String(volts) + " mV | ";
  toPrint += String(current) + " mA | ";
  toPrint += String(capacity) + " / ";
  toPrint += String(fullCapacity) + " mAh | ";
  toPrint += String(power) + " mW | ";
  toPrint += String(health) + "%";

  Serial.println(toPrint);

  // LCD Graphics
  tft.setTextColor(TFT_BLUE);
  tft.drawRoundRect(10, 10, 300, 220, 10, TFT_BLUE);
  tft.setTextColor(TFT_MAGENTA);
  tft.drawString("State of Chage:", 20, 30);
  tft.drawString("Battery Voltage:", 20, 55);
  tft.drawString("Average Current:", 20, 80);
  tft.drawString("Remain Capacity:", 20, 105);
  tft.drawString("Full Capacity:", 20, 130);
  tft.drawString("Average Power:", 20, 155);
  tft.drawString("State of Health:", 20, 180);

  // Data
  spr.createSprite(80, 170);
  spr.fillSprite(TFT_BLACK);
  spr.setFreeFont(FF17);
  spr.setTextColor(TFT_WHITE);
  spr.drawString(String(soc)+" % ", 0, 0);
  spr.drawString(String(volts)+" mV ", 0, 25);
  spr.drawString(String(current)+" mA ", 0, 50);
  spr.drawString(String(capacity)+" mAh ", 0, 75);
  spr.drawString(String(fullCapacity)+" mAh ", 0, 100);
  spr.drawString(String(power)+" mW ", 0, 125);
  spr.drawString(String(health)+" % ", 0, 150);
  spr.pushSprite(170, 30);
  spr.deleteSprite();
}

void setup()
{
  Serial.begin(115200);
  tft.begin();
  tft.setRotation(3);
  tft.fillScreen(TFT_BLACK);
  tft.setFreeFont(FF17); 
  setupBQ27441();
  tft.setTextColor(TFT_GREEN);
  tft.setCursor((320 - tft.textWidth("Battery Initialised!"))/2, 120);
  tft.print("Battery Initialised!");
  delay(1000);
  tft.fillScreen(TFT_BLACK);
}

void loop() 
{
  printBatteryStats();
  delay(1000);
}

  • Sign in to reply

Top Comments

  • genebren
    genebren over 5 years ago +2
    Interesting device. The datasheet on the BQ27441 mentions a Coulomb counter, which would imply that the charge and discharge currents (mA) are being used to accumulate the charge over time (mAH) to determine…
  • Jan Cumps
    Jan Cumps over 5 years ago +2
    I've used a bq27510-G2. Time to review that again. These gauges are a great way to keep track of charge and health...
  • ralphjy
    ralphjy over 5 years ago in reply to genebren +1
    Thanks, I'll go read that white paper. The thing that confused me - still does - about the battery capacity is that the program sets that value in a register using lipo.setCapacity(BATTERY_CAPACITY). I…
  • ralphjy
    ralphjy over 5 years ago in reply to Jan Cumps +1
    I haven't used a battery fuel gauge before, but I'd also not encountered PMICs until having to reprogram one on the Ultra96v2 board. Now I see PMICs being used on even low cost boards and I'll probably…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to ralphjy +1
    ralphjy wrote: ... I'd also not encountered PMICs until having to reprogram one on the Ultra96v2 board. Now I see PMICs being used on even low cost boards and I'll probably want to use those and these…
  • genebren
    genebren over 5 years ago in reply to ralphjy +1
    Ralph, I have looked through the datasheet and through the SparkFunBQ27441 library and I am completely confused. The library does not seem to match the datasheet. There is a lot to be confused about, as…
  • ralphjy
    ralphjy over 5 years ago in reply to genebren +1
    Gene, Thanks for taking a look. I definitely want to get to the bottom of this, but it will have to wait a bit. This was supposed to be a quick diversion from working on Vibration Sensor data. I guess…
  • ralphjy
    ralphjy over 5 years ago in reply to genebren

    Thanks, I'll go read that white paper.  The thing that confused me - still does - about the battery capacity is that the program sets that value in a register using lipo.setCapacity(BATTERY_CAPACITY).

    I haven't seen any reference about how the fuel gauge uses that 650 mAh value that is programmed.  Likewise can't see a reference to how the State of Health is determined although from what I've read I'd expect a value closer to 100% for a new battery rather than 0%.  Anyway, still nice to monitor battery voltage and current.  I was able to get a new schematic.  I was hoping that the GPOUT pin would be connected to one of the MCU pins so that I could use it as a low voltage interrupt, but it only comes out to a test point so I'd have to open it up and modify it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    I've used a bq27510-G2. Time to review that again. These gauges are a great way to keep track of charge and health...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago

    Interesting device.  The datasheet on the BQ27441 mentions a Coulomb counter, which would imply that the charge and discharge currents (mA) are being used to accumulate the charge over time (mAH) to determine the actual battery charge state.  In a product that I worked on we did the same sort of process, with current and voltage monitoring, to drive a charge indicator (LEDs).  When properly calibrated we were able to get a pretty good readout of the remaining charge in the battery.

     

    TI has a white paper (slpy002) that describes in better detail their ImpedanceTrackTm algorithms, which appear to use Coulomb counting, impedance measurements, open-circuit battery voltages and various table to predict the battery charge level.  The Aging value seems to be based on long term changes in the measured capacities across multiple charge/discharge cycles, so you might have to wait a bit to see a change in that reading.

     

    With Li-Ion batteries, the listed capacity can vary widely compared to the actual capacity of the battery.  The displayed capacity of 584mAH is within ~10% of the rated capacity, so this is not too surprising.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<