Member and Staff Blogs Year of the Monkey Badge: Zao Jun
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 29 Jan 2016 10:34 AM Date Created
  • Views 4442 views
  • Likes 9 likes
  • Comments 55 comments
  • chinese_new_year
  • year_of_the_monkey
  • kitchen
  • cooking
Related
Recommended

Year of the Monkey Badge: Zao Jun

spannerspencer
spannerspencer
29 Jan 2016

Year of the MonkeyCelebrate Chinese New Year with element14!

 

Day Six: Zao Jun

 

Nimen hao! We're now sprinting toward the Year of the Monkey, and it's time to start preparing for all the visitors and feasting! And who better to help out than Zao Jun, the Kitchen God?

 

But first, it's the Year of the Monkey, so in order to win our time-limited badge, all you need to do is stop by to read and comment on each of our New Year blogs. The badge will only be available to earn until February 23, after which you'll have to wait 12 years before it comes up again (given the cycle of the Chinese zodiac).

 

What's Cooking in Your Kitchen?

Zao Jun is an interesting chap. He's the God of the Kitchen, which sounds quite passive in most respects. But he actually has something of a sinister, authoritarian remit.image

 

During the Chinese New Year celebrations, people burn paper effigies of Zao Jun, but not to punish him. It whisks him away to the nether realm so he can report on you and your family to the Jade Emperor (who runs heaven) about all your good deeds and transgressions. A kind of naughty and nice list, if you like.

 

One method of encouraging Zao Jun to give a more favourable report is by offering up sweet foods, like candy and confectionery. But maybe there are other options, like coming up with some awesomely clever electronics project for the kitchen. What can you think of that'd help out with those culinary tasks, or revolutionise your kitchen experience? Tell us, and therefore Zao Jun, all about it!

  • Sign in to reply

Top Comments

  • peterjcs23
    peterjcs23 over 10 years ago +4
    my favourite cake, do have a virtual piece: Peter
  • lahcen005
    lahcen005 over 10 years ago +4
    how about two robot helping hand?
  • pettitda
    pettitda over 10 years ago in reply to jack.chaney56 +2
    Ever come up with a solution to a problem that only existed in your dream?
  • COMPACT
    COMPACT over 10 years ago in reply to wolfmountaingames +1
    That doesn't work! I'm very fussy about my fresh produce and don't want to let others pick or mishandle it.
  • COMPACT
    COMPACT over 10 years ago +1
    Before the days of the tablet, we've got a handy quantity converter and calculator. It can convert imperial to metric and vice versa and it can also perform ingredient quantity adjustments for recipes…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    How about an egg timer that can tell when the egg is correctly boiled, no idea how to acheive that but im sure density and temperature and time will factor into it Maybe a bit of ultrasonics ?? A protien…
  • dougw
    dougw over 10 years ago +1
    How about some kind of small radiant heat lid to cook the top side of a fried egg, so you don't have to flip it over....
  • Workshopshed
    Workshopshed over 10 years ago +1
    An analyser to show how many coffee's I had that day and adjust caffeine levels accordingly.
  • bwelsby
    bwelsby over 10 years ago +1
    As I am now retired and my wife still working I tend to do most of the cooking in our house and the biggest problem is deciding what to cook. I would like a database of all the meals we like which is linked…
  • srpsco
    srpsco over 10 years ago +1
    I am quite tall, especially compared to everyone else in the house. I would love to see an adjustable height counter top. A little frame with some linear actuators.
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    How about an egg timer that can tell when the egg is correctly boiled, no idea how to acheive that but im sure density and temperature and time will factor into it

     

    Maybe a bit of ultrasonics ??

     

    A protien re-sequencer (Replicator)... how cool would that be

     

    or for a simpler thing, a receipe program that works with ratios instead of absolute ingredient weight, this way you can scale to what ever you want based on what you have, not what you need

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago in reply to Robert Peter Oakes

    I also want a replicator. Do those require a Heisenberg Compensator, the same as the transporters?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to spannerspencer

    AFAIK (which is very little) there are two main types of replicator.

    One has a tank of sub atomic particles held in suspension in dark matter fluid and a beam of highly focused dark energy is used to link together the particles into the atoms and molecules for the required product which is built up layer by layer. These do not require the Heisenberg Compensator.

    The other type uses a technique involving quantum entanglement to copy objects held in cloud storage and these do require a Heisenberg Compensator.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bwelsby
    bwelsby over 10 years ago in reply to spannerspencer

    AFAIK (which is very little) there are two main types of replicator.

    One has a tank of sub atomic particles held in suspension in dark matter fluid and a beam of highly focused dark energy is used to link together the particles into the atoms and molecules for the required product which is built up layer by layer. These do not require the Heisenberg Compensator.

    The other type uses a technique involving quantum entanglement to copy objects held in cloud storage and these do require a Heisenberg Compensator.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • spannerspencer
    spannerspencer over 10 years ago in reply to bwelsby

    Ah, that's useful info, yeah. I assumed they worked much like a transporter, but instead of repositioning the deconstructed material, the replicator rematerialised a quantity of subatomic particles into matter to construct different, pre-determined forms. Like food, drinks (Tea. Earl Grey. Hot.) or machine parts. Obviously you couldn't recreate things with a complex quantum structure this way (that's just crazy talk) but it'd be useful when operated in reverse too, so rather than having to do the washing up you could just destroy the plate's molecules.

     

    However they work, I'd quite like to have one.