Member and Staff Blogs Year of the Monkey: Guan Yu and Me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 29 Jan 2016 10:32 AM Date Created
  • Views 3750 views
  • Likes 8 likes
  • Comments 50 comments
  • guan_yu
  • chinese_new_year
  • year_of_the_monkey
Related
Recommended

Year of the Monkey: Guan Yu and Me

spannerspencer
spannerspencer
29 Jan 2016

Year of the MonkeyCelebrate Chinese New Year with element14!

 

Day Five: Guan Yu and Me

 

Nimen hao! Perhaps you remember our Christmas advent calendar shenanigans, when members of the element14 team all gave away their deepest, darkest secrets, and we asked you to guess which skeletons belonged in which closet?

 

Well, one of my fun facts was a long-time love of kung fu, and I mention it now in the midst of our Chinese New Year celebrations as today's patron is someone I'm very familiar with from those kung fu classes. He's the Chinese God of War, and a very popular figure when the New Year rolls around.

 

But first, it's the Year of the Monkey, so in order to win our time-limited badge, all you need to do is stop by to read and comment on each of our New Year blogs. The badge will only be available to earn until February 23, after which you'll have to wait 12 years before it comes up again (given the cycle of the Chinese zodiac).

 

Romance of the Three Kingdoms

We won't get into a debate about the existence of gods here, but a unique aspect of the Chinese God of War, Guan Yu (or Guan Gung, as he's also known) is that he really did exist. His epic exploits saw him become the subject of one of China's greatest works of literature of all time (The Romance of the Three Kingdoms), and his subsequent ascension into being a recognised deity.image

 

When you position your Guan Yu statue in your house (and every respectable house has such a statue, of course) he's positioned to face the door. This prevent bad luck, demons and those of ill intention from being able to enter your dominion.

 

So in honour of Guan Yu in the New Year, we want to hear your thoughts on new or existing security-focused projects. Digital security, physical security, personal security -- any clever ways to make the world a safer place through the magic of electronics!

  • Sign in to reply

Top Comments

  • lahcen005
    lahcen005 over 10 years ago +4
    what I find is secure USB drive like see the two examples below.
  • dougw
    dougw over 10 years ago +3
    Fingerprints were used in ancient times, maybe as far back as 1000 BC. In ancient China they were used for identification and as signatures, and there is currently a surge in popularity, as fingerprint…
  • ntewinkel
    ntewinkel over 10 years ago +3
    We just had to replace the keypad entry on our guest house because one of the keys failed. boo. Yes just one, complete failure of a single digit. That's what we get for having the security code "1111"…
  • cstanton
    cstanton over 10 years ago +3
    At Leeds Hackspace one of the members created our entire entry system using Arduino's and electronic locks with an RFID system. So you get an RFID card and pin number, which is used for the outer door…
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago +3
    A robotic python that roams around and moves to areas where movements is detected. Some people have problems with baboons and they are terrified of snakes.
  • mzungu
    mzungu over 10 years ago in reply to spannerspencer +2
    spannerspencer - Haven't 'gone off grid' - there is no grid here - at least, within a reasonable distance - quote from power company to supply, USD50,000 - cost of my solar setup, USD2,000. I have 6 panels…
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to mzungu +2
    Where are you when you are off the grid. For me I just got back from Michigan's Upper Peninsula. About 120 miles by about 300 miles, and a single area code. Spotty phone, mostly 3G when available.
  • mzungu
    mzungu over 10 years ago in reply to jack.chaney56 +2
    Sorry jack.chaney56 , I must learn to be more precise! (slaps own wrist!). The DC side of the solar is 24V, supplying some loads directly, and 230VAC loads via an inverter. The pump is a 250W submersible…
  • e14 Contributor
    e14 Contributor over 10 years ago +1
    nice description ~
  • COMPACT
    COMPACT over 10 years ago +1
    I'll only allow the use of bamboo computers!
  • mzungu
    mzungu over 10 years ago in reply to mcb1

    Great idea, Mark.  The pump runs on 230VAC from the inverter - getting 24VDC down to the pump 100 metres away would cost too much copper to run a DC pump - but I did have the foresight to run an old cat5 cable to the pump.  So your idea will still work, if I entangle the cat5 cores around the pump so it is impossible to remove without breaking the loop, then run the 24VDC down the loop, and through the opto (got a few kicking around somewhere...). The photodiode in the opto can then keep a transistor off by pulling down the base.  When the loop is broken, a pullup resistor on the base can turn on the tr, and hence a relay (got a box full of 24VDC coil relays - literally a box full (left over from an old project!)) to activate any interesting 'siren' I can find (I have an old 12V one somewhere...).

     

    Power consumption in the quiescent state should be insignificant ( <100mW, I would guess)

     

    Ahhhhh - I feel good today image

     

    Thanks again, Mark.

    Cheers,

    Tony

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • momososo
    momososo over 10 years ago

    More security need more time or more high speed MCU means more money.

    Maybe raspberry pi zero will be good to solution this problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    An extension of my eLDERMON project that included front door monitoring as well as external PIR activity might be a start.

    This could trigger a RPi camera to record the front door visitor.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to mzungu

    You should be able to run a normally closed system, which uses the earth connection, or the negative on the pump to keep the input LED on an optocoupler energised.

    The current can be quite low depending on which opto you use.

     

    I run a similar system on the skifield trip system and they are 1km away using telephone cable .

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 10 years ago

    There are myriad sensors that can be employed to detect intruders. A facial recognition project would also be a great experience.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>