• Products and Partners
    Products and Partners
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
Holiday Secret Santa Entries Automatic Wire Strippers are great gifts!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 3 Jan 2022 5:52 AM Date Created
  • Views 2747 views
  • Likes 16 likes
  • Comments 9 comments
  • secretsanta
Related
Recommended

Automatic Wire Strippers are great gifts!

ntewinkel
ntewinkel
3 Jan 2022

Happy Holidays Everyone!

If you're a few weeks behind like I am, here is a great belated gift for anyone working with electronics: automatic wire strippers.

What makes them great is that they just happily do the job of stripping the insulation off the wire without us having to know the size of the wire - it magically just knows!

These Jokari T20050 (Newark part number33P8621) ones are really nice:

Jokari Wire Strippers

https://www.newark.com/jokari/t20050/automatic-wire-stripper-super4/dp/33P8621?st=automatic%20wire%20stripper

Hopefully SecretSanta 2021 will help bring these to someone who can really put them to good use!

Seasons Greetings and Happy New Year!

  • Sign in to reply

Top Comments

  • dougw
    dougw over 4 years ago +5
    It would be nice to see an in depth study on wire stripping tools - they are important. I have a bunch of types and I have used a bunch at work and I almost always end up using the cheapest ones I have…
  • fmilburn
    fmilburn over 4 years ago +2
    A great idea! I have been manually gauging length and setting wire diameter for years.
  • robogary
    robogary over 4 years ago +2
    Nice productivity tool. Thanks for the tip.
Parents
  • dougw
    dougw over 4 years ago

    It would be nice to see an in depth study on wire stripping tools - they are important. I have a bunch of types and I have used a bunch at work and I almost always end up using the cheapest ones I have (with a set of needle nose pliers to hold the wire). It seems I am often stripping in tight quarters where a big fancy stripper can't fit, or there isn't enough wire for the big stripper to grip, or the fancy stripper is a bit out of calibration for the type of wire I am stripping, or it simply doesn't work as well as the cheap strippers. How can a semi-automated stripper do a cable where only only a very short section of wire extends out of the cable (because the backshell needs to grip the bigger cable jacket). If someone has found a really good solution that works for 22 gage through 32 gage in tight locations, I would be interested in seeing a review.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to dougw

    Hi Doug,

    I don't know of any single truly universal wire stripper for all wire and insulation types, but almost all of the above requirements are met by Knipex 12 12 02 - it exceeds the wire size range you mention, easily supporting 16 to 32 AWG. There is a blog discussing its sibling model 12 12 06 here  (near-identical tool but for a different wire range). 

    Both are really good, I use them regularly, however another good tool with just slightly less range on either end of the range you specify, it covers 24 to 30 AWG, is Stripmaster 45-672 which I mention because its head is much smaller than the Knipex tools, to meet your tight spot needs. I prefer the Stripmaster tool all general PCB wiring, especially 30 AWG Kynar wire, which it feels purpose-built for, it is so good on that. I use it with thicker general equipment wire too, e.g. typical stranded wire. It's no good for (say) inside-chassis mains wiring, for which I move to the Knipex tool since it supports the thicker wires.

    Incidentally, on all of these tools mentioned, you can strip sections of wire that are maybe just 15mm long, i.e. the wires are so short you'd have to hold the wire with tweezers and feed one end into the wire stripper. So, it's possible to prepare ultra-short length wires with just a couple of mm stripped off either end, no problem at all with these styles of wire strippers.

    They cut amazingly well, no comparison with the stamped-metal notch types. (However for building/home mains wiring, the tools mentioned above are overkill and not ideal.. instead, I like the pliers with notches shaped for the wire, they are super-quick on the PVC insulation that is expected for that scenario).

    No single tool unfortunately, but the Kipex one and especially the Stripmaster if you can sacrifice one gauge on either end : ) would appear to be closest from my perspective.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 4 years ago in reply to dougw

    Hi Doug,

    I don't know of any single truly universal wire stripper for all wire and insulation types, but almost all of the above requirements are met by Knipex 12 12 02 - it exceeds the wire size range you mention, easily supporting 16 to 32 AWG. There is a blog discussing its sibling model 12 12 06 here  (near-identical tool but for a different wire range). 

    Both are really good, I use them regularly, however another good tool with just slightly less range on either end of the range you specify, it covers 24 to 30 AWG, is Stripmaster 45-672 which I mention because its head is much smaller than the Knipex tools, to meet your tight spot needs. I prefer the Stripmaster tool all general PCB wiring, especially 30 AWG Kynar wire, which it feels purpose-built for, it is so good on that. I use it with thicker general equipment wire too, e.g. typical stranded wire. It's no good for (say) inside-chassis mains wiring, for which I move to the Knipex tool since it supports the thicker wires.

    Incidentally, on all of these tools mentioned, you can strip sections of wire that are maybe just 15mm long, i.e. the wires are so short you'd have to hold the wire with tweezers and feed one end into the wire stripper. So, it's possible to prepare ultra-short length wires with just a couple of mm stripped off either end, no problem at all with these styles of wire strippers.

    They cut amazingly well, no comparison with the stamped-metal notch types. (However for building/home mains wiring, the tools mentioned above are overkill and not ideal.. instead, I like the pliers with notches shaped for the wire, they are super-quick on the PVC insulation that is expected for that scenario).

    No single tool unfortunately, but the Kipex one and especially the Stripmaster if you can sacrifice one gauge on either end : ) would appear to be closest from my perspective.