Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Dimmer repair
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 77 replies
  • Subscribers 41 subscribers
  • Views 14574 views
  • Users 0 members are here
Related

Dimmer repair

wal_e
wal_e over 5 years ago

Hello everyone,

First of all I would like to apologize, I might certainly be in the wrong section, but I have been sent here by the Farnell technical assistance and to be honnest this place is a real maze for me image

So, I have been trying to fix a dimmer that went working only as a simple switch : OFF to ON max light directly. Following my researches it seems that the origin of my problem is a faulty triac and also - maybe - a capacitor ; I have tested both of the 2 fuses and they are ok.

The two original component are labeled:

- BTB04-600A

- CBB62B X2 0.033µF (250-280VAC) dimensions 40/110/56/C

My problem is that I can't find any of the exact two components and I have no idea what I can use to replace them as equivalent.

Any help is really appreciated

Thank you - very much - in advance.

 

W

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5
    Hi, If rotating the dimmer makes it turn the light on and off, then why do you think the triac is faulty? Couldn't it be the rotary potentiometer? (I don't know - I'm speculating). I'm not sure it is good…
  • jw0752
    jw0752 over 5 years ago +4
    Hi Walid, If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when…
  • wal_e
    wal_e over 5 years ago in reply to shabaz +4
    Hello Shabaz, Thank you for taking the time to answer. I found this diagnostic on the internet, it says that if the dimmer only works from OFF to ON max power it's a triac issue. As you can imagine this…
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Walid,

     

    If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when the dimmer is removed from power by checking the continuity between A1 and A2 terminals. It should be open under normal circumstances. If it is shorted then the triac is bad. The other components are probably OK. The BTB 04-600A is a 4 Amp 600 Volt triac and can be replaced with pretty much any triac that has ratings of more than 4 amps and 600 volts. I have some BTB 06-600 which would be 6 amps and 600 volts. If you are inside the USA I will send one to you. If you are looking at the triac with the pins down and the label facing you the A1 and A2 terminal are the left pin and the center pin. The right pin is the gate and should be attached to a DB3 trigger diode if you have a standard design.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    Thank you for your help I really appreciate your kind answer but I am too far from you that would make this triac very expensive image So, I am experiencing exactly what you described and already replaced the old triac with a new one labeled BTB08-600BW (the only "equivalent" triac I found in the neiborhood) which didn'ty solve the problem. So I just tested both of them and both of their A1 and A2 show no continuity....does that mean they're both open and ok ? When I tested the capacitor I got a 0.0µF instead of 0.033µF...is it possible that my tester is not sensitive enough or is my capacitor is dead ? In that case could he be the origin of the problem ?

    Best regards,

     

    W

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Hi Walid,

     

    I looked a little closer at the standard dimmer circuit and the capacitor is also quite important. My schematic shows a 0.33 uF but that is probably for 115 VAC and you are probably working with 230 VAC. If your meter can check capacitors the 0.033 should not be too small for it to read. It should indicate 33 nF. I was wrong before about testing the Diac. It should not show any resistance in either polarity on your ohmmeter. Diacs do not break down and trigger until they are in the area of 30 V plus.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    My meter is digital and unfortunatly not a fancy one...I tested both triacs, BTB04-600A shows 1.9 mega ohm between A1 and A2 and goes to 0.6 kilo ohm when A2 and Gate shorted. BTB08-600BW shows 13.3 mega ohm and then 80 ohm when A2 and gate shorted.

    I tested again the original box capacitor and it shows 0µF instead of 0.033 µF (or OL?). I have a spare polypropylene capacitor marked 333K (and 400VMY) which should be 0.033 µF but when tested it shows 677 µF :/

    I found another spare polypropylene capacitor marked 103K (and 630 FN) and showing 0.1 µF when tested, maybe this one could replace the original one ?

    What do you think ?

    Thank you in advance.

    W

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    wal_e  wrote:

     

    Hi John,

    My meter is digital and unfortunatly not a fancy one...I tested both triacs, BTB04-600A shows 1.9 mega ohm between A1 and A2 and goes to 0.6 kilo ohm when A2 and Gate shorted. BTB08-600BW shows 13.3 mega ohm and then 80 ohm when A2 and gate shorted.

     

     

    The TRIAC measurements are OK

     

     

    I tested again the original box capacitor and it shows 0µF instead of 0.033 µF (or OL?). I have a spare polypropylene capacitor marked 333K (and 400VMY) which should be 0.033 µF but when tested it shows 677 µF :/

    I found another spare polypropylene capacitor marked 103K (and 630 FN) and showing 0.1 µF when tested, maybe this one could replace the original one ?

    What do you think ?

    Thank you in advance.

    W

     

    OL is usually range overload. That means that te capacity is higher than the DMM can show in the active range.

    33 nF is typically supported by a DMM. Does your meter have an option to change range for capacity measurements?

    333K is 33 nF, So that is a good one.

     

     

    I found another spare polypropylene capacitor marked 103K (and 630 FN) and showing 0.1 µF when tested, maybe this one could replace the original one ?

    That's also an off measurement. 103K should be 0.01 µF / 10 nF.

    I would not put a 10 nF where the 33 nF is expected ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    Hi Jan,

    So I can solder back the original triac on the pcb ?

    My DMM has auto range selection I can't change anything, in the manual, for capacitance it says :

    Measuring range 600 µF -> résolution 0.1 µF

    Measuring range 6000 µF -> résolution 1 µF

    In both cases: accuracy : +- 4% reading + +3digits

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to wal_e

    So I tried putting back the original triac and replacing the capacitor with the 333K and it didn't work...same problem: from OFF to ON max power but no dimming function...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Did you test the DIAC. Small cylindrical component with two leads that is between the gate of the Triac and the capacitor?

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Did you test the DIAC. Small cylindrical component with two leads that is between the gate of the Triac and the capacitor?

     

    John