Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Dimmer repair
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 77 replies
  • Subscribers 41 subscribers
  • Views 14621 views
  • Users 0 members are here
Related

Dimmer repair

wal_e
wal_e over 5 years ago

Hello everyone,

First of all I would like to apologize, I might certainly be in the wrong section, but I have been sent here by the Farnell technical assistance and to be honnest this place is a real maze for me image

So, I have been trying to fix a dimmer that went working only as a simple switch : OFF to ON max light directly. Following my researches it seems that the origin of my problem is a faulty triac and also - maybe - a capacitor ; I have tested both of the 2 fuses and they are ok.

The two original component are labeled:

- BTB04-600A

- CBB62B X2 0.033µF (250-280VAC) dimensions 40/110/56/C

My problem is that I can't find any of the exact two components and I have no idea what I can use to replace them as equivalent.

Any help is really appreciated

Thank you - very much - in advance.

 

W

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5
    Hi, If rotating the dimmer makes it turn the light on and off, then why do you think the triac is faulty? Couldn't it be the rotary potentiometer? (I don't know - I'm speculating). I'm not sure it is good…
  • jw0752
    jw0752 over 5 years ago +4
    Hi Walid, If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when…
  • wal_e
    wal_e over 5 years ago in reply to shabaz +4
    Hello Shabaz, Thank you for taking the time to answer. I found this diagnostic on the internet, it says that if the dimmer only works from OFF to ON max power it's a triac issue. As you can imagine this…
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Walid,

     

    If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when the dimmer is removed from power by checking the continuity between A1 and A2 terminals. It should be open under normal circumstances. If it is shorted then the triac is bad. The other components are probably OK. The BTB 04-600A is a 4 Amp 600 Volt triac and can be replaced with pretty much any triac that has ratings of more than 4 amps and 600 volts. I have some BTB 06-600 which would be 6 amps and 600 volts. If you are inside the USA I will send one to you. If you are looking at the triac with the pins down and the label facing you the A1 and A2 terminal are the left pin and the center pin. The right pin is the gate and should be attached to a DB3 trigger diode if you have a standard design.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    Thank you for your help I really appreciate your kind answer but I am too far from you that would make this triac very expensive image So, I am experiencing exactly what you described and already replaced the old triac with a new one labeled BTB08-600BW (the only "equivalent" triac I found in the neiborhood) which didn'ty solve the problem. So I just tested both of them and both of their A1 and A2 show no continuity....does that mean they're both open and ok ? When I tested the capacitor I got a 0.0µF instead of 0.033µF...is it possible that my tester is not sensitive enough or is my capacitor is dead ? In that case could he be the origin of the problem ?

    Best regards,

     

    W

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    The knob that you turn to select dim or bright is a variable resistor. It has two terminals that attach at the edge of the board.  When it is at dim I would expect a reading of several hundred K Ohms . When it is at the bright position I would expect a low Ohm reading.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    That knob is also used to go from OFF to min light, at that point (even when in off position) it reads 14.6 when DMM is in 20 Kohm and when max bright light it reads 1.8 when DMM is in 200 ohm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    See if you can remove the solder from one leg of the control so that it is separated from the circuit trace. Try the dimmer with power on. The light should stay off. Unplug the unit and check the resistance of the control again with the one leg still detached. When you read the meter watch to see if a "K" is displayed with the number on the display. What are the minimum and maximum position resistances?

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John, I "drew" the circuit of the dimmer. Here the control is labeled P and has 3 legs: 2 that you can see on the other photos and one under it. Please let me know which one I should remove the solder from.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    Walid, can you double-check the circuit around the potentiometer P and R1?

    On your circuit that looks like a dead end. It only has one wire connected to the circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    Hi Jan, sorry I indeed forgot some part of the circuit but it doesn't involve the paret you pointed. Here is a corrected drawing and the photo of the back circuit annotated.

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to wal_e

    My mistake, phase in is lower. Here is corrected:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Hi Walid,

    The two connections at the center of the board are the ON OFF switch . If you can remove the solder from either of the other connections at the edge of the board so that the metal leg from the P control no longer touches the copper you will be able to perform my experiment. Nice job on drawing the schematic. I am not sure that it is totally correct as the switch isn't where I would expect to see it in the circuit but who knows. This experiment is to verify that the control is working properly. Once the leg of P is no longer touching the circuit copper traces you will have to touch the meter to the two legs to get the resistance readings.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Thank you John. Am I supposed to test it while light is at max light or dim ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    We need to get a resistance reading on the two legs closest to the edge of the board in the dim position and the bright position. Make certain there is no power to the system when these readings are made or you may damage the meter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    We need to get a resistance reading on the two legs closest to the edge of the board in the dim position and the bright position. Make certain there is no power to the system when these readings are made or you may damage the meter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    The holes are too narrow the legs are still touching the pcb...I am going to take it away and test it away from the circuit is that still ok ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Sure that will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    I have to leave for a while. I will check back in a couple hours.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Okay, here are the mesures:

    Max light: 1.7 when DMM is on 200 ohm

    Min light: 16.8 when DMM is on 20 Kohm

    OFF: oscilating between 16.8 and 17.5 when DMM is on 20 Kohm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    My first question is: Did this dimmer ever work to your knowledge?

     

    Your readings on the variable resistor are 20 times smaller than what I would expect them to be in this design. Is it possible that this unit is a manufacturing defect where they accidentally installed a 20K variable control when they intended to install a 400K?

     

    Do you happen to have a high ohm potentiometer like a 500 K that we could patch into the circuit to see if we can get it to dim. If you have such a potentiometer let me know and i will tell you how to patch it in to verify this theory. As i am sure you already know you have to be careful as we are dealing with hazardous and possibly fatal voltage levels in this circuit.

     

    By the way your excellent technical skills have made this troubleshooting adventure a lot of fun.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Thank you John image I remember it working perfectly yes. When you asked about the 500K potentiometer, I remember seeing this on the one installed : B500K

    image

    This can't only be a coincidence right ? So how this could be malfunctionning ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    Great sleuthing, John. +- 17K for a 500K potentiometer is indeed off.

     

    Walid, the potentiometer upper housing and shaft are plastic for your safety - it's wired to your power outlet without isolation.

    I'd advise to use an equally well isolated one, if you are going to replace it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    I started to look for an equivalent on the internet...most of the ones I saw have 3 front legs :/

    Just out of curiosity, isn't it possible to fix it ? Or at least to try to understand what happened to it?

    For your information, as a novice, I certainly tried an economic bulb at some point...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    It is very very unusual for a control to change value. I have seen situations where too much current has damaged and changed controls but usually the resistance goes up and not down. If the control had some sort of contaminate that was an electrolyte spilled on it the resistance might come down. If you can find a replacement, which may be a challenge, you could raise the metal tabs on the body and open the control up to see if anything internally is evident. By the way you can turn any of the three legged potentiometers into a two legged one by cutting off one lead.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    It seems that this one would do the job :

    https://www.amazon.fr/gp/product/B07MLFX3Y4/ref=ox_sc_act_title_1?smid=A38WCF64ZZVDKC&psc=1

    Now I will begin the disassembly to to take a look inside and will get back to you.