Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Dimmer repair
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 77 replies
  • Subscribers 41 subscribers
  • Views 14345 views
  • Users 0 members are here
Related

Dimmer repair

wal_e
wal_e over 5 years ago

Hello everyone,

First of all I would like to apologize, I might certainly be in the wrong section, but I have been sent here by the Farnell technical assistance and to be honnest this place is a real maze for me image

So, I have been trying to fix a dimmer that went working only as a simple switch : OFF to ON max light directly. Following my researches it seems that the origin of my problem is a faulty triac and also - maybe - a capacitor ; I have tested both of the 2 fuses and they are ok.

The two original component are labeled:

- BTB04-600A

- CBB62B X2 0.033µF (250-280VAC) dimensions 40/110/56/C

My problem is that I can't find any of the exact two components and I have no idea what I can use to replace them as equivalent.

Any help is really appreciated

Thank you - very much - in advance.

 

W

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5
    Hi, If rotating the dimmer makes it turn the light on and off, then why do you think the triac is faulty? Couldn't it be the rotary potentiometer? (I don't know - I'm speculating). I'm not sure it is good…
  • jw0752
    jw0752 over 5 years ago +4
    Hi Walid, If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when…
  • wal_e
    wal_e over 5 years ago in reply to shabaz +4
    Hello Shabaz, Thank you for taking the time to answer. I found this diagnostic on the internet, it says that if the dimmer only works from OFF to ON max power it's a triac issue. As you can imagine this…
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Sure that will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    I have to leave for a while. I will check back in a couple hours.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Okay, here are the mesures:

    Max light: 1.7 when DMM is on 200 ohm

    Min light: 16.8 when DMM is on 20 Kohm

    OFF: oscilating between 16.8 and 17.5 when DMM is on 20 Kohm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    My first question is: Did this dimmer ever work to your knowledge?

     

    Your readings on the variable resistor are 20 times smaller than what I would expect them to be in this design. Is it possible that this unit is a manufacturing defect where they accidentally installed a 20K variable control when they intended to install a 400K?

     

    Do you happen to have a high ohm potentiometer like a 500 K that we could patch into the circuit to see if we can get it to dim. If you have such a potentiometer let me know and i will tell you how to patch it in to verify this theory. As i am sure you already know you have to be careful as we are dealing with hazardous and possibly fatal voltage levels in this circuit.

     

    By the way your excellent technical skills have made this troubleshooting adventure a lot of fun.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Thank you John image I remember it working perfectly yes. When you asked about the 500K potentiometer, I remember seeing this on the one installed : B500K

    image

    This can't only be a coincidence right ? So how this could be malfunctionning ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    Great sleuthing, John. +- 17K for a 500K potentiometer is indeed off.

     

    Walid, the potentiometer upper housing and shaft are plastic for your safety - it's wired to your power outlet without isolation.

    I'd advise to use an equally well isolated one, if you are going to replace it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    I started to look for an equivalent on the internet...most of the ones I saw have 3 front legs :/

    Just out of curiosity, isn't it possible to fix it ? Or at least to try to understand what happened to it?

    For your information, as a novice, I certainly tried an economic bulb at some point...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    It is very very unusual for a control to change value. I have seen situations where too much current has damaged and changed controls but usually the resistance goes up and not down. If the control had some sort of contaminate that was an electrolyte spilled on it the resistance might come down. If you can find a replacement, which may be a challenge, you could raise the metal tabs on the body and open the control up to see if anything internally is evident. By the way you can turn any of the three legged potentiometers into a two legged one by cutting off one lead.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    It seems that this one would do the job :

    https://www.amazon.fr/gp/product/B07MLFX3Y4/ref=ox_sc_act_title_1?smid=A38WCF64ZZVDKC&psc=1

    Now I will begin the disassembly to to take a look inside and will get back to you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    I just thought of another possibility. It is possible that the wiper inside the control has come loose from the shaft and has limited mobility near the low end. Bend the metal tabs up and open the control and check it out. You can also test the carbon strip by putting your meter from one end to the other. I bet we will see 500K or there abouts. If the wiper is loose perhaps you can fix the control by reattaching it.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>