Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Novice in trouble
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 39 subscribers
  • Views 1807 views
  • Users 0 members are here
  • trouble
  • in
  • novice
Related

Novice in trouble

e14 Contributor
e14 Contributor over 12 years ago

Hi all. I'm a retired mechanic and have VERY little knowledge in the magic that is electronics. So I'm throwing myself on to you good people who can maybe help me out.

   I hate throwing stuff away that could easily be repaired with a little bit of effort. I was given a golf trolley last year that didn't work. It has a module with a circuit board inside that looks like it has got wet at some time. I've tested the transistors (only 3) and found 1 of them has blown. The numbers on it are HO1 and YM3045N. I've tried to find one on the net but failed. Is there a way of finding an equivalent. From my limited knowledge it looks like it controls the voltage to the motor. Secondly would water getting into it be enough to blow it or should I look for a popped diode or something as well?..... Thanks in advance ... Bill

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    A google search reveals that the YM.. identifier is a dual rectifier, not a transistor. Water could have damaged bits of the circuit. What's worse, if it was powered up while wet, then yes there could be more serious damage. If there is a programmed device on board then if that is damaged there is almost no hope of repair without the manufacturer's help. Perhaps it didn't work before the water damage, in which case there is even more guesswork.

    It may be difficult to repair without some test equipment and electronics knowledge, and even then it might not be possible without manufacturer support. Not really sure what more can be said, engineering is a huge topic (can take years of study) and without more information it's hard to advise much. If there are things that are clearly faulty (e.g. burned tracks, fuses blown etc) then sometimes visual inspection can help, and an approximate idea what each area of the board might do, and the problem symptoms based on visual inspection and some measurements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    A google search reveals that the YM.. identifier is a dual rectifier, not a transistor. Water could have damaged bits of the circuit. What's worse, if it was powered up while wet, then yes there could be more serious damage. If there is a programmed device on board then if that is damaged there is almost no hope of repair without the manufacturer's help. Perhaps it didn't work before the water damage, in which case there is even more guesswork.

    It may be difficult to repair without some test equipment and electronics knowledge, and even then it might not be possible without manufacturer support. Not really sure what more can be said, engineering is a huge topic (can take years of study) and without more information it's hard to advise much. If there are things that are clearly faulty (e.g. burned tracks, fuses blown etc) then sometimes visual inspection can help, and an approximate idea what each area of the board might do, and the problem symptoms based on visual inspection and some measurements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    Thank you for your reply shabaz... I have checked the parts of this board that I can. Diodes resisters etc and can't fault them. It has a small I.C that I don't know how to check and wouldn't know how to replace anyway. I am working on the theory, if it only costs me a couple of £'s to try a new (Dual Rectifier???? I don't know what that is) part then I don't mind trying. I have looked on a site that shows how to test this part and there are no connections within. My little knowledge of such things tells me that a replacement is prolly available. As I said it was given to me and I hate seeing things wasted so I haven't lost anything i trying to repair it. Another answer on here suggests it is a NPN transistor. which is what I first assumed it was. Is a dual rectifier the same?...Or am I just being DUMB?