• Products and Partners
    Products and Partners
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
Member's Forum Using Multiple Ultrasonic Sensors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 632 subscribers
  • Views 1174 views
  • Users 0 members are here
  • new_member_introduction
Related

Using Multiple Ultrasonic Sensors

grondak
grondak over 7 years ago

I'd like to build a robot with three sensors for left, front, and right distances.   I'd like to ensure that the output signal of one sensor doesn't get picked up by the others' receivers.  Any ideas here? A physical "horn" to ensure selective hearing (heh)?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    As Michael indicates, this is normally handled with sequential activation. This slows response time so sometimes it is not ideal. Best speed is achieved by using the return from one sensor to trigger the start of the next device.

    Another method is to use different frequencies for each sensor direction. This requires different narrow band sensors for each direction.

    It may be also possible to send from a single omni directional transmitter and have separate receivers for each direction. This could still result in a reflected signal arriving before a long return, depending on geometries involved - that needs to be assessed.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • grondak
    grondak over 7 years ago in reply to dougw

    Many of the ultrasonic sensors that are easy to buy have a single circuit board with a transceiver pair.  I searched online for a simple way to change the frequency on such boards but didn't find one right away.  Is there a method that you've seen for this?

     

    Also I like the sequential trigger idea.  An interrupt from receipt could read the timer and initiate the next device, in a ring.  Thank you!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to grondak

    The low cost sensor pairs with electronics use tuned transmitters and receivers so they can only work at the designed frequency,

    I've never seen  a low cost system that used different frequencies to separate sensors.

     

    The 10x figure is a good rule of thumb, based on trying to measure reversing sensors and arrays of them in lab conditions. Once you get your system working you can experiment with  a bit of tuning of the interval.

    The problem with triggering in a ring is that depending on the target the first echo may well not be as big a a later echo from a different target and that the varying time between measurements may well cause problems at a system level.

     

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • grondak
    grondak over 7 years ago in reply to michaelkellett

    I suspect the next thing to do is to actually write the software and tune it with a test rig. Maybe I'll get to it this weekend!

    I'll post the Arduino or CircuitPy sketch up here for discussion when I do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • grondak
    grondak over 7 years ago in reply to michaelkellett

    I suspect the next thing to do is to actually write the software and tune it with a test rig. Maybe I'll get to it this weekend!

    I'll post the Arduino or CircuitPy sketch up here for discussion when I do.