Member's Forum How can you manage to damage a soldering iron like this?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 632 subscribers
  • Views 3945 views
  • Users 0 members are here
  • soldering tips
  • soldering iron
  • soldering
Related

How can you manage to damage a soldering iron like this?

cstanton
cstanton over 7 years ago

image

My first thought is, perhaps it's corrosion, from high or excess heat, these are disposable parts after all, but what really contributes to this kind of wear, and is there anything that can be done to prevent it being so sudden or so soon?

 

Often I find the soldering tips in the workstation to be bent, or the end of the tip looking like it's snapped off.

 

What're your thoughts?

How long do tips last for you or how often do you replace them?

What do you use to take care of your soldering iron?

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    Pictures really tell a lot in a thread like this so here are my irons and a collection of old tips:

    image

    The Aoyue is the iron part of my hot air rework station - I don't use the iron part much, because it isn't as good as the Hakko I use most of the time (I didn't bring the whole Hakko over for the picture).

    The blue tip in the middle is the one I am currently using in the Hakko.

    The Tenma is new, courtesy of element14 - only used in my camera area so far.

    The Yong Feng looks unused because it is - I bought it for $12 - it might see some use for mobile work since the temperature control is in the handle, eliminating the big controller block.

    Some of the tips have a worn spot that doesn't "wet" with solder well but I don't throw them out in case I want to use them for melting PLA or hot glue or some other application that would mess up a nice tip.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dougw

    dougw  wrote:

     

    ...

    Some of the tips have a worn spot that doesn't "wet" with solder well but I don't throw them out ...

    For those cases, I use these two:

    image

    As you can see, I don't use it often. Only when I create spots that don't wet (typically when melting a connector away with the iron because "it needs to go" image )

    The polish bar and activator are not to be used when the tip is OK. They are not maintenance utilities, but repair. They have downsides.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dougw

    dougw  wrote:

     

    ...

    Some of the tips have a worn spot that doesn't "wet" with solder well but I don't throw them out ...

    For those cases, I use these two:

    image

    As you can see, I don't use it often. Only when I create spots that don't wet (typically when melting a connector away with the iron because "it needs to go" image )

    The polish bar and activator are not to be used when the tip is OK. They are not maintenance utilities, but repair. They have downsides.

    • Cancel
    • Vote Up +6 Vote Down