• Products and Partners
    Products and Partners
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
Member's Forum A Simple Continuity Tester
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 630 subscribers
  • Views 598 views
  • Users 0 members are here
  • continuity tester
  • continuity
Related

A Simple Continuity Tester

1cm69ltd
1cm69ltd over 6 years ago

Hi all,

 

I am an amateur hobbyist currently messing around with Arduino/ESP8266 boards & have made a number of simple data loggers for around my house.

 

I found that my current DMM, a Bryman BM235 has a relatively high continuity cut-off, 30 to 480 Ohms & this has caused me an issue lately as I suspected a short in one of my loggers but this particular logger had a 150 Ohms resistor which my DMM did not even see.

 

Searching the net for a simple alternative I came across a straight forward schematic: Continuity Tester

 

Initially I constructed this circuit on a breadboard & it did not function, no sound when touching the probes together. I tried the various troubleshooting steps laid out on the page with no success. I even swapped transistors, checked all the actual resistor & capacitor values butr it still did not function.

 

I decided that it could possibly be an issue with the breadboard in some way & then constructed the circuit on some protoboard.

 

Still the same result or should I say no result, I get nothing from the tester.

 

Through fault finding I found that shorting between B & E of Q1 gives an audible tone but that's it so I know the buzzer is working.

 

I took a few readings from the circuit:

 

Input Voltage: 3.278v

Across Buzzer: 2.699v

Across 100R: 0.446v

On Probe: 0.758v

Base Q3: ~ 2.7v

Across Diodes: 2.055v

Probe leads resistance: 7 ohms

 

Can anyone see a possible glaring error with this circuit that I am unable to see.

 

Regards..,

 

Kirk

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    What's the DC collector-emittor voltage over Q1 with the probes open and closed?

    Did you use a PNP transistor for Q3?

    Voltage accross the buzzer should be AC.

    Removing Q1 should turn on the buzzer all the time. If it doesn't, the issue is with the Q2/Q3 circuit.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 6 years ago

    What's the DC collector-emittor voltage over Q1 with the probes open and closed?

    Did you use a PNP transistor for Q3?

    Voltage accross the buzzer should be AC.

    Removing Q1 should turn on the buzzer all the time. If it doesn't, the issue is with the Q2/Q3 circuit.