• Products and Partners
    Products and Partners
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
Member's Forum Is anyone interested with the Z80?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 151 replies
  • Subscribers 648 subscribers
  • Views 10853 views
  • Users 0 members are here
  • z80
Related

Is anyone interested with the Z80?

COMPACT
COMPACT over 10 years ago

The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    What sort of things would you discuss - Z80 has such poor performance compared with modern processors that surely no one would use one in  a new project ?

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to michaelkellett

    Would you believe the Z80 is still in production today?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to COMPACT

    I know it's still being made but so are spares for Ford Model T !

     

    My question was about using one in a new project, is there any reason why one would ?

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 10 years ago in reply to COMPACT

    I know it's still being made but so are spares for Ford Model T !

     

    My question was about using one in a new project, is there any reason why one would ?

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • COMPACT
    COMPACT over 10 years ago in reply to WarrenW

    So what's watching the watchdogs, and what's watching the watchdog's watchdogs, and what's watching the watchdog's watchdog's watchdog?.....

     

    A zap of uncontrolled ESD can put it all at risk.

     

    How did Toyota and other car manufacturers get some of their code so wrong to cause safety issues?

    MISRA standards are only a starting point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenW
    WarrenW over 10 years ago in reply to Workshopshed

    Safety Applications?

    What would you be looking at doing? Most off the shelf safety controllers used in industrial applications that require certification (very few safety applications don't!) are dual processors with watchdogs to each from each to ensure that it all behaves according to plan.

     

    If you want to certify this application for use then there is a very long road ahead to get certification to the relevant standards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to COMPACT

    Programmable logic excels at counting image

     

    Have a nice day !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to michaelkellett

    Programmable logic doesn't count because it can be applied to both!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to COMPACT

    I'll raise your 50MHz ........

     

    https://en.wikipedia.org/wiki/WDC_65C02

     

    image

     

    re provability  - I told you no one cared - the VIPER was a total flop (and that's about how fast it was image)

     

    It's interesting that when people have built fast versions of old architectures it hasn't turned out to be good business - remember Scenix and the 100MHz PIC ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to michaelkellett

    I've used both of these micros and you're trying to compare apples and lychees.

    Each micro has its own strengths and weaknesses.

    The most important thing is whether you can accomplish your desired task quickly and easily.

     

    VHDL, Verilog and programming models don't necessarily tell you the real story about what's inside the ICs!

    To do that you have to look at the actual die designs.

     

    These processors were aimed at different markets.

    The Z80 was specifically designed to be backward compatible with the Intel 8080 so that it could immediately run a vast amount of software. About 60% of its die is dedicated for instruction decoding. It also has built in DRAM refresh support.

    The 6502 used a different approach. It is a cheap clone of the 6800 and due to its lower price was used by many manufacturers.

    The Apple ][ needed a plug in Z80 board to access the loads of Z80 CP/m software.

     

    One obvious reason why the Z80 uses more transistors than a 6502 is because it has four times as many registers than the 6502) and that means lots more transistors are needed.

     

    As for speed, did you know the Z80 can exchange the contents of two 16 bit registers in 4 T states. That's 1uS @ 4MHz.

    Later versions of the Z80 can run up to 50MHz with single cycle execution - That's 20ns for the 16 bit register exchange instruction. Try that with a 6502!

    (If a 4GHz version were built it'd be 250ps!)

     

    As for stack size and flexibility the Z80 can have its stack located at any memory location and be of any size. The 6502 has a fixed size of 256 bytes at a fixed address.

     

    As for provability NASA must of thought it cut the mustard because the Z80 was used on the Space Shuttle.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to michaelkellett

    The 6502 was used in the schools BBC Micro but strangely enough we never

    looked at the individual transistors when I was at school.

    We did at uni but not that processor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to COMPACT

    For teaching you are better off with the 6502, much nicer design (IMO), far fewer transistors, full VHDL/Verilog models available.

     

    @Andy, probably far easier to "prove" a modern design like Cortex M0. In the dim and distant past "proveably correct " micros have been designed but they flopped totally.

     

    https://en.wikipedia.org/wiki/VIPER_microprocessor

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to COMPACT

    That also raises the question, of can it be totally modelled in software and hence all cases proved out.

    Am thinking of safety applications

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to michaelkellett

    Ah but from the original company?

     

    Yes, as a teaching device. The Z80 only consists of about 10,000 transistors hand laid without CAD.

    But if these could be made using today's transistors (say 14nm) should yoctoscopic and draw next to no power!