• Products and Partners
    Products and Partners
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
Member's Forum Is anyone interested with the Z80?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 151 replies
  • Subscribers 648 subscribers
  • Views 10819 views
  • Users 0 members are here
  • z80
Related

Is anyone interested with the Z80?

COMPACT
COMPACT over 10 years ago

The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.

  • Sign in to reply
  • Cancel
  • COMPACT
    COMPACT over 8 years ago in reply to dougw

    image

    If you want to build a small real Z80 system then you could just deploy a single Zilog Z84C15 Highly Integrated Z80 IPC (Integrated Peripheral Controller).

    It has inbuilt SIO, CTC and PIO and runs at 16Mhz

    Just add RAM, Flash and your desired electrical interfaces - The pictured system has TCP/IP Ethernet capabilities, runs CP/M, has two true RS232 ports, 2 PIO parallel ports and some Timer Counters .

    Alternatively you could use an eZ80 which can run at 50MHz with single cycle instruction fetch.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to balearicdynamics

    Very cool balearicdynamics - I'll have to think up some project that justifies building one of these....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 8 years ago

    A Z80 is still in production (incredible image ) this guy has done an incredibly great job :The Z80 Membership Card Computer

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 8 years ago in reply to gdstew

    That is the latest document from Zilog but beware! It contains transcription errors in its diagrams and text.

     

    The Z80 also provides in-built Dynamic RAM (DRAM) refresh support which limits its performance.

    Later Z80 derivatives can run without DRAM support

    The first of these is the HD64180 where one can tune or even turn off DRAM support for improved performance.

     

    Even later Z80 derivatives have single cycle instruction fetch.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to dougw

    The Slit-N-Wrap wire is 28AWG and normally 30AWG is used for Wire Wrapping.

    I usually use 24, 26 and 28AWG for prototyping because I find that 30AWG is a bit too flimsy.

    Dobs of glue are also useful for holding wires in place.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jgerred
    jgerred over 9 years ago in reply to Workshopshed

    I agree with Workshopshed, I programmed in assembly many years ago but would have very little (if anything) to contribute to a current discussion.  I would most likely follow it as time permits, but hand jamming assembly code no longer tops my list!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to gdstew

    I still have a motorized Slit-N-Wrap and I still use it once in a while. It used to be really fast for wiring low-speed backplanes - much faster than manually soldering connectors on PCBs. I built a circuit that would make it automatically stop wrapping after 7 turns.

    I never had problems with shorts. They have 2 types of wire, one with a Tefzel (Teflon) jacket that is thicker than normal Kynar, the other is  a thin green enamel coating (a bit like magnet wire). I never had problems with either type although I was always careful not to let the green stuff rub on square pins.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 9 years ago in reply to COMPACT

    Yes, three voltage power supplies ruled then. And you can add +24V for the 8" floppy drives but they were usually in their own case with a separate

    +5V, +24V power supply. The MK4116, and all other dynamic RAMs of the time used +5V, +12V, -5V which was usually derived from the -12V which

    came in handy for  RS-232RS-232 drivers

     

    I thought it was Slit-N-Wrap but I couldn't remember so I went for the long version. I thought Vector was still around, I wonder if they fixed the shorting

    problem ?

     

    I remember the Just Wrap too and I know I was very interested but for some reason, lost in the mists of time, I never bought one which is made even

    more curious after all the Slit-N Wrap problems. I think I just went to pre-cut wire wrap wire (which I still cut to length) with an electric wire wrap tool but ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to gdstew

    Ahhh!

     

    The days of triple power supplies (+5, +12 and -12V).

     

    Slit-N-Wrap from Vector.

    It's still available today but not on the e14 catalogue.

     

    I used a competing product called JUST WRAP and I think I've still got the blighter!

    Ok Wire Wrap Jw-1-w Just Wrap 0.25 Daisy Chain Or Point To Point Nib Handheld

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 9 years ago in reply to COMPACT

    No photos but the schematics were from a Mostek Z80 application note which I may still have. I used a tool from Vector called the Slit and Wrap which used

    small spool of wire coated with a soft insulator kind of like magnet wire that was slit by the wrap bit just before it was wrapped on the post. It was a great tool

    for speeding up wire wrapping with one fatal flaw. If two wires pressed against each other hard enough, they could displace the soft insulator and short.

    When ever I powered it up and it did not work I would have to look for two wires pressed against each other in a rats nest of wires (actually I was more

    systematic than that but there were always problem areas) and separate them. When the offending wires were separated it would usually make a distinctive

    "plink" sound so I knew when I found it.

     

    I used the same tool and a Z80 to wrap up a 256 x 240 x 4 bit/pixel graphics display controller. The schematic was from Byte Magazine and I modified it from

    the original 1 bit/pixel configuration and to use static RAMs that were fast enough to allow the Z80 full speed access to the video RAM by interleaving the

    accesses with video timing generator. The Z80 assembly language software had to be entered in by hand to be assembled and of course modified to handle

    the multi-bit/pixel mod and to use a 8 bit parallel interface to the SDB-80. I believe it only had commands for pixel read/write, line and circle drawing.

    Unfortunately after quite a few sessions of find the Slit and Wrap short I gave up and disassembled it for the parts and never used my Slit and Wrap again.

     

    Like I said, fun (and sometimes frustrating) days.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
<>