Member's Forum Electronics for Theremins (1)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 632 subscribers
  • Views 2046 views
  • Users 0 members are here
  • tutorial
  • theremin
Related

Electronics for Theremins (1)

FredM
FredM over 15 years ago

This is the resource page to accompany  the thread Electronics for Theremins – 1 –
which is running at http://www.thereminworld.com/Forums/T/26581/electronics-for-theremins---1

 

General discussion on this matter should be done at the Theremin World forum (link above) but suplimentary data / schematics etc can be attached / hosted here by members of this group.. If you have not yet signed up to E-14, do so now!  Joining this group is free, and Element-14 is a great site for technical matters.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • FredM
    FredM over 13 years ago

    This posting is a response to several email requests from people who have a problem understanding coil windings, particularly with regard to phase relationships. Below the phase dots are shown for a coil / transformer, and the equivalent schematic diagram given - together with calculations.

     

    An online calculator is available from Pace Magnetics here: http://powermagnetics.co.uk/calculator.html

    image

     

    image

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FredM
    FredM over 13 years ago in reply to FredM

    I found this crude test oscillator I built years ago to test SRF of inductors -

     

    This is based on the EM theremin design by Bob Moog - It is a wonderfully reliable oscillator, and clipping an inductor between +Vout and TST one will usually get oscillations at aproximately the SRF of the inductor.

     

    I put the transistors in sockets, as it is possible to blow them up if one connects something stupid - I also put sockets to allow a capacitor to be connected across the inductor.

     

    A simple, basic but useful piece of kit for theremin developers.

     

    image

    Layout on 0.1" pad board:

     

    Pads G1 and G2 are ground, VP1 is STABLE +12V, VN1 is STABLE -12V, Out is to 'scope / frequency counter, VP2 is +V supply to inductor, TST is to other side of inductor. Note that the TST lead is an "antenna" - it needs to be short.. The OUT signal will be low level unless into a high-Z input - the 100k is in series to reduce the effect of the measuring instrument, but this isnt ideal.

    Layouts viewed from component side (top).

    image

    Pads shown:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to FredM

    Great blog! Why no folks on tho? Thanks Fred.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 11 years ago in reply to FredM

    Great blog! Why no folks on tho? Thanks Fred.