Member's Forum Compensating / "linearizing" an RC oscillator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 631 subscribers
  • Views 1253 views
  • Users 0 members are here
  • vfo
  • linearity
  • compensating
  • theremin
  • rc
  • oscillator
  • 555
Related

Compensating / "linearizing" an RC oscillator

FredM
FredM over 14 years ago

It is well known that the worst form of oscillator to use as a theremin VFO is the RC type - The frequency of these oscillators is simply a function of R*C, and as the "antenna" to hand capacitance follows an inverse square law, pitch (from heterodyning the VFO with a fixed reference oscillator) response (linearity) is the worst possible.

 

LC oscillators without an equalizing inductor have a better response, and this is greatly improved (in most cases) by adding a suitable series inductor with the antenna..

 

The circuit presented here has only been evaluated (not extensively) in simulation - It has not yet been built. The objective is to improve the "linearity" of a simple RC oscillator used as a theremin VFO.

 

image

In the above implementation which uses a TS555CD.TS555CD. as the oscillator, C1 RV1 and R2 form a 'monostable' type circuit which changes the charging and discharging paths for C2 (the antenna capacitance) - The effect of these components is to increase the frequency as the frequency increases - as in, if C2 reduces, the frequency will increase to a greater degree than would have occurred if C1 had not been present.

 

Waveforms shown below give a better understanding of the operation:

 

image

Shown are waveforms for an antenna capacitance of 22pF and 23pF, with linearity control set to 50% and 100%. It should be noted that the Tuning potentiometer (VR) and the linearity potentiometer are highly interactive. For higher VFO frequencies, C1 should be reduced.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 14 years ago

    Hi Fred,

     

    Good post.  The Theramin always gets my interest.  I will have to play around with some 555 circuits to see what else I can generate out of the different signals.

     

    Plus, you are right about copyright and patents.  They just give you the recourse to sue if you detect someone using your product without your permission.

    Which implies that A. you have to find out if anyone is doing it.  and B.  Is it worth your while to engage a lawyer to sue.

     

    Only large companies have the resources to pursue such action and even they do a cost benefit analysis before proceeding.  Often, you just send a cease and desist order to get them to either stop, or ask permission to use you device and negotiate a royalty.

     

    Thanks for sharing.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 14 years ago

    Hi Fred,

     

    Good post.  The Theramin always gets my interest.  I will have to play around with some 555 circuits to see what else I can generate out of the different signals.

     

    Plus, you are right about copyright and patents.  They just give you the recourse to sue if you detect someone using your product without your permission.

    Which implies that A. you have to find out if anyone is doing it.  and B.  Is it worth your while to engage a lawyer to sue.

     

    Only large companies have the resources to pursue such action and even they do a cost benefit analysis before proceeding.  Often, you just send a cease and desist order to get them to either stop, or ask permission to use you device and negotiate a royalty.

     

    Thanks for sharing.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • FredM
    FredM over 14 years ago in reply to DAB

    Hi DAB,

     

    What follows is a rant! LOL!

     

    IMO, the whole patent process has now reach a stage where it actually holds back progress. One of the reasons I now publish my ideas (even trivial ones) is that the only reasonably safe way one can protect ones ideas is to put them into the public domain - I have fallen foul of patent abuse once in the past - I incorporated an idea into one of my designs which was put into production by my employer, and large volumes of this product were sold - Then, years after production had started, a large competitor reverse engineered the product and patented my idea. Because my idea had never been patented (I never dreamed it was worth patenting) or published, the patent was granted - and the competitor then sued my employer for infringment! It seemed like nonsence, but the competitors legal resources allowed them to force the company I was working for to stop production of 'my' product, and caused the company to go bancrupt.

     

    Following this I researched for similar cases (I simply could not believe this could have happened) and found many - Some quite famous like EMI vs GE(USA) where GE {in my opinion} blatantly stole patented IP (related to body scanner) from EMI.

     

    The greatest perversion of the patent system, IMO, is the patenting of gene sequences produced by evolution - Decoding a gene sequence is not inventing, it is discovering! Oh, I wish there was a god who descended with 'his' legal team and took these b**tards to task! LOL!

     

    Fred.