Member's Forum e14 membership tops 200,000
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 633 subscribers
  • Views 655 views
  • Users 0 members are here
Related

e14 membership tops 200,000

e14 Contributor
e14 Contributor over 13 years ago

There are currently 200,474 e14 members, with about 1000 new members added every 6 days.

 

14,724 (7.3%) are at level 1 or above (which requires 2 or more points).

  2,905 (1.4%) are at level 2 or above (which requires 51 or more points).

  1,415 (0.7%) are at level 3 or above (which requires 101 or more points).

     518 (0.3%) are at level 4 or above (which requires 301 or more points).

     198 (0.1%) are at level 5 or above (which requires 1001 or more points).

     141 (0.07%) are at level 6 or above (which requires 1501 or more points).

     118 (0.06%) are at level 7 or above (which requires 2001 or more points).

       82 (0.04%) are at level 8 or above (which requires 3001 or more points).

       64 (0.03%) are at level 9 or above (which requires 4001 or more points).

       49 (0.02%) are at level 10 or above (which requires 5001 or more points).

 

Of the 200,474, 155,819 are external, 2017 are internal, 1004 are supplier,

and 41,634 are unspecified.

 

Half the members joined since May, 2012.

The RPi group has 8,947 members (4.5%).

 

Countries represented (top 12):

60773   US

27236   UK

19750   China

  9349   Germany

  8633   India

  6804   Canada

  6159   Australia

  5822   France

  4126   Italy

  4051   Spain

  3992   Netherlands

  3406   Poland

  • Sign in to reply
  • Cancel
Parents
  • Nate1616
    Nate1616 over 13 years ago

    Thanks for the post Coder27.  Very interesting stats.  It would be interesting to see why so many are at level one.  Is it because they are afraid to ask a question or answer one.  If thats the case maybe we need to do something about it.  Now what that is im not sure.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Nate1616
    Nate1616 over 13 years ago

    Thanks for the post Coder27.  Very interesting stats.  It would be interesting to see why so many are at level one.  Is it because they are afraid to ask a question or answer one.  If thats the case maybe we need to do something about it.  Now what that is im not sure.

     

    Nate