Member's Forum going from LiPo battery to wall power?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 632 subscribers
  • Views 2780 views
  • Users 0 members are here
  • android
  • charge
  • battery
  • tablet
  • power
Related

going from LiPo battery to wall power?

e14 Contributor
e14 Contributor over 11 years ago

I'm trying to run a tablet I have that runs on a 3.7v battery off of the wall directly without a battery. Reason is my sister broke the charging cable, and thus I decided to convert it to an android TV of some sort. I got a buck converter and I set it to 3.7v but the tablet doesn't turn on! it flashes on for a second and then turns off. I tried using different amp measurements, but all that did was keep the screen on a few fractions of a second more before it turns off again

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Ehab,

    I suspect that the circuit that maintains and monitors the battery is shutting the unit down when it detects that the battery is missing. Where are you attaching the 3.7 volts? To the charger Mini USB port or directly to the battery contacts? As long as your power supply has enough current capacity the voltage is all that matters. The unit will draw the current that it needs from the 3.7 volts. If you have a meter you can monitor the voltage when you turn the unit on. You may need a good capacitor on the output of your buck supply so and surge demand of the unit doesn't cause it to pull the power down momentarily. Some batteries have more connections than just the + and - power. If your battery has more than 2 connections the unit may need the battery in the circuit in order to power up.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Thank you for the response!
    I have connected the buck converter's output directly to the battery pins (there are only 2 pins). if it makes any difference, I'm providing the converter with an input of 5v. You mentioned that I need to connect a capacitor to the output of the buck converter. How much exactly? I don't really know the formula to calculate that image
    oh, and the battery that came with the tablet is 3.7V 7800mAh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Ehab,

    5 volts input to the 3.3V converter might be a little low. Usually they need at least 2 volts higher input than output. I would start with a 470 uF capacitor at any voltage 10 volts or higher. If you have a way to measure the voltage of the converter when you turn on the unit you will be able to see if it can maintain the 3.3 volts required. If it drops below 3 volts you can try a 6 or a 7 volt supply to your converter. If you battery had only 2 terminals then we should be able to get this to work. Connecting to the battery terminal is what I would do too. Also on hooking up the capacitor make sure the plus lead of the capacitor goes to the plus lead of the converter and the negative lead of the capacitor goes to the negative lead of the converter.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I found this information:

     

    Module Spec: non-isolated step-down (BUCK)

    Rectification: non-synchronous rectification

    Input voltage: 4V-35V

    Output voltage: 1.23V-30V

    Output Current: 3A (max)

    Conversion efficiency: 92% (the highest)

    Switching frequency: 150KHz

    Output ripple: 30mV (max)

    Load Regulation: ± 0.5%

    Voltage Regulation: ± 2.5%

    Operating Temperature: -40 ℃ to +85 ℃

    The peripheral dimensions: 48 * 23 * 14 (L * W * H) (mm)

    Notes: Default output is 20V from factory setting.

     

    LM2596 Power Module

     

     

    it seems like the 12v input is ok, so I'll try that in a bit. However, I'm curios; does the switching frequency have anything to do with this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Ehab Charek wrote:

     

    I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

     

    Unfortunately I don't know, you'd need to check with the vendor of your DC-DC converter.

    I'm all out of ideas I'm afraid!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I've added the capacitor to the circuit as mentioned by John as of yesterday. Which, according to you, means that it could either be the power supply, or the buck converter. I am, in fact, using a converter I got from ebay. I am also using a power supply I got from a flea market, as I don't have another one with 6-7 volts of output. I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

    Mark, as for your suggestion, the button works with no issues when the tablet is running off the battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    According to this site

    http://www.pipomall.com/index.php?main_page=faq_info&faqs_id=112

    image

     

    Is it possibly the open/close button causing the issue.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    According to your earlier post you're connecting your power supply to the terminals where the battery connects. And you just have a 2-pin battery.

    In that case, the issue is likely to be your power supply/DC-DC converter. If it is a cheap e-bay one then it may not be able to supply sufficient current, or may need the capacitor as mentioned by John.

    If these tips don't help, you probably need to investigate further and supply more detail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    it works perfecty fine when running off the battery

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    it works perfecty fine when running off the battery

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I found this information:

     

    Module Spec: non-isolated step-down (BUCK)

    Rectification: non-synchronous rectification

    Input voltage: 4V-35V

    Output voltage: 1.23V-30V

    Output Current: 3A (max)

    Conversion efficiency: 92% (the highest)

    Switching frequency: 150KHz

    Output ripple: 30mV (max)

    Load Regulation: ± 0.5%

    Voltage Regulation: ± 2.5%

    Operating Temperature: -40 ℃ to +85 ℃

    The peripheral dimensions: 48 * 23 * 14 (L * W * H) (mm)

    Notes: Default output is 20V from factory setting.

     

    LM2596 Power Module

     

     

    it seems like the 12v input is ok, so I'll try that in a bit. However, I'm curios; does the switching frequency have anything to do with this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Ehab Charek wrote:

     

    I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

     

    Unfortunately I don't know, you'd need to check with the vendor of your DC-DC converter.

    I'm all out of ideas I'm afraid!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I've added the capacitor to the circuit as mentioned by John as of yesterday. Which, according to you, means that it could either be the power supply, or the buck converter. I am, in fact, using a converter I got from ebay. I am also using a power supply I got from a flea market, as I don't have another one with 6-7 volts of output. I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

    Mark, as for your suggestion, the button works with no issues when the tablet is running off the battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    According to this site

    http://www.pipomall.com/index.php?main_page=faq_info&faqs_id=112

    image

     

    Is it possibly the open/close button causing the issue.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    According to your earlier post you're connecting your power supply to the terminals where the battery connects. And you just have a 2-pin battery.

    In that case, the issue is likely to be your power supply/DC-DC converter. If it is a cheap e-bay one then it may not be able to supply sufficient current, or may need the capacitor as mentioned by John.

    If these tips don't help, you probably need to investigate further and supply more detail.