Member's Forum going from LiPo battery to wall power?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 632 subscribers
  • Views 2755 views
  • Users 0 members are here
  • android
  • charge
  • battery
  • tablet
  • power
Related

going from LiPo battery to wall power?

e14 Contributor
e14 Contributor over 11 years ago

I'm trying to run a tablet I have that runs on a 3.7v battery off of the wall directly without a battery. Reason is my sister broke the charging cable, and thus I decided to convert it to an android TV of some sort. I got a buck converter and I set it to 3.7v but the tablet doesn't turn on! it flashes on for a second and then turns off. I tried using different amp measurements, but all that did was keep the screen on a few fractions of a second more before it turns off again

  • Sign in to reply
  • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to mcb1

    Hi Mark,

    Thanks for your insight. I personally have tried to circumvent an integrated battery in a piece of equipment. You are undoubtedly right as it apparently isn't working.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to jw0752

    John

    Many of the tablets use 15v to charge the battery (they detect the device and up the output voltage), so its possible the battery management electronics is deciding the battery is not there or is depleted based on use and charging.

     

    Maybe some info on the actual tablet model might help in overcoming the issue.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    hello there!
    sorry for the late response, I was busy with finals, and the capacitor took its sweet time to arrive. I did what you told me to do, but it did not change anything, however. I added the capacitor, and increased the input voltage, but it's still having the issue.

    I also measured the voltage as it was booting up, and it was dropping, but only by a little bit. It goes from 3.80v to 3.72v, and it does not go lower than that. from what I understand, a completely charged lipo battery should have a voltage of around 4v, and a discharged one should have a voltage of 3.0v. The measurements I'm getting are in between, so they should be ok?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Ehab,

    5 volts input to the 3.3V converter might be a little low. Usually they need at least 2 volts higher input than output. I would start with a 470 uF capacitor at any voltage 10 volts or higher. If you have a way to measure the voltage of the converter when you turn on the unit you will be able to see if it can maintain the 3.3 volts required. If it drops below 3 volts you can try a 6 or a 7 volt supply to your converter. If you battery had only 2 terminals then we should be able to get this to work. Connecting to the battery terminal is what I would do too. Also on hooking up the capacitor make sure the plus lead of the capacitor goes to the plus lead of the converter and the negative lead of the capacitor goes to the negative lead of the converter.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Thank you for the response!
    I have connected the buck converter's output directly to the battery pins (there are only 2 pins). if it makes any difference, I'm providing the converter with an input of 5v. You mentioned that I need to connect a capacitor to the output of the buck converter. How much exactly? I don't really know the formula to calculate that image
    oh, and the battery that came with the tablet is 3.7V 7800mAh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago

    Hi Ehab,

    I suspect that the circuit that maintains and monitors the battery is shutting the unit down when it detects that the battery is missing. Where are you attaching the 3.7 volts? To the charger Mini USB port or directly to the battery contacts? As long as your power supply has enough current capacity the voltage is all that matters. The unit will draw the current that it needs from the 3.7 volts. If you have a meter you can monitor the voltage when you turn the unit on. You may need a good capacitor on the output of your buck supply so and surge demand of the unit doesn't cause it to pull the power down momentarily. Some batteries have more connections than just the + and - power. If your battery has more than 2 connections the unit may need the battery in the circuit in order to power up.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<