Member's Forum going from LiPo battery to wall power?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 632 subscribers
  • Views 2754 views
  • Users 0 members are here
  • android
  • charge
  • battery
  • tablet
  • power
Related

going from LiPo battery to wall power?

e14 Contributor
e14 Contributor over 11 years ago

I'm trying to run a tablet I have that runs on a 3.7v battery off of the wall directly without a battery. Reason is my sister broke the charging cable, and thus I decided to convert it to an android TV of some sort. I got a buck converter and I set it to 3.7v but the tablet doesn't turn on! it flashes on for a second and then turns off. I tried using different amp measurements, but all that did was keep the screen on a few fractions of a second more before it turns off again

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I found this information:

     

    Module Spec: non-isolated step-down (BUCK)

    Rectification: non-synchronous rectification

    Input voltage: 4V-35V

    Output voltage: 1.23V-30V

    Output Current: 3A (max)

    Conversion efficiency: 92% (the highest)

    Switching frequency: 150KHz

    Output ripple: 30mV (max)

    Load Regulation: ± 0.5%

    Voltage Regulation: ± 2.5%

    Operating Temperature: -40 ℃ to +85 ℃

    The peripheral dimensions: 48 * 23 * 14 (L * W * H) (mm)

    Notes: Default output is 20V from factory setting.

     

    LM2596 Power Module

     

     

    it seems like the 12v input is ok, so I'll try that in a bit. However, I'm curios; does the switching frequency have anything to do with this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Ehab Charek wrote:

     

    I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

     

    Unfortunately I don't know, you'd need to check with the vendor of your DC-DC converter.

    I'm all out of ideas I'm afraid!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I've added the capacitor to the circuit as mentioned by John as of yesterday. Which, according to you, means that it could either be the power supply, or the buck converter. I am, in fact, using a converter I got from ebay. I am also using a power supply I got from a flea market, as I don't have another one with 6-7 volts of output. I do have, however, a few good 12v power supplies. Is it safe to use those instead?

     

    Mark, as for your suggestion, the button works with no issues when the tablet is running off the battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    According to this site

    http://www.pipomall.com/index.php?main_page=faq_info&faqs_id=112

    image

     

    Is it possibly the open/close button causing the issue.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    According to your earlier post you're connecting your power supply to the terminals where the battery connects. And you just have a 2-pin battery.

    In that case, the issue is likely to be your power supply/DC-DC converter. If it is a cheap e-bay one then it may not be able to supply sufficient current, or may need the capacitor as mentioned by John.

    If these tips don't help, you probably need to investigate further and supply more detail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    it works perfecty fine when running off the battery

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Are you sure the tablet actually works? Perhaps there is a fault causing it to immediately power off.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to jw0752

    Sorry I mistyped  - I meant to say I have never personally tried to circumvent an integrated battery so I am not the best person to be answering this question.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    thanks for the reply!
    the tablet is a chinese one made by a company called PIPO. And the model is the Pipo M9. here's the battery for that tablet:

    Original 3.7V 7800mAh Rechargeable Lithium Battery For PIPO M9 Tablet - US$37.26

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to jw0752

    Hi John,

     

    I think this is a likely issue. There are often three or more connections, one being a thermistor in the battery pack. With that absent, the power management IC won't start up the device.

    Tablets have fairly big batteries so there may be a third connection somewhere. We need to know the tablet model. According to youtube teardowns, even supermarket-branded tablets can have more than two connections to the battery pack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>