• Products and Partners
    Products and Partners
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
Member's Forum Iphone charging...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 60 replies
  • Subscribers 634 subscribers
  • Views 6079 views
  • Users 0 members are here
  • usb
  • 5vdc
  • iphone
Related

Iphone charging...

e14 Contributor
e14 Contributor over 11 years ago

Hello, my name is Martin
I have a very big problem with a 5v usb boost circuit. When i connect the circuit to the power, the led lights up, but no power... to iphones... everything else works, just not iphones. i already tried shorting the data ports with the 5v pin, AND THAT USED TO WORK, but not now!!!??

PLEASE HELP

I have now tried with adding some resistors to data+ and minus, still nothing image

 

HELP!!!

 

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You need to make a resistor dividers to both D+ and D- lines: http://cdn.instructables.com/FOF/IG95/GTLRHJWG/FOFIG95GTLRHJWG.LARGE.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Im not sure if i understood correctly. This picture shows the device i have, and what you're telling me, is that somewhere, i have to add 4 resistors?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Exactly. iphone charges only when d+ and d- are pulled to about 2.7v. I cannot exactly remember if those voltages are absolutely correct.

    Normal USB charger just won't work for that reason.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to e14 Contributor

    Yes it only requires a sniff of power it's only setting a data line after all not shunting any power through it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Now that i applied resistors the phone says "this accesory may not be supported " please help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    *kinda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    Well yeah, i Linda figured that wasnt alot, so im asking. Should i go for 3aa's? 4? And should i connect Them in series like they usually are or in parallel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    What are you powering that circuit with?

    A couple of AA batteries? It will take a long time to charge your phone if so.

    The resistors connect to the USB D+ and D- lines and to the 5V and 0V connections. In the link that Petri showed, the USB connector is shown on the right (i.e. corresponds to the USB connector on your board), and the two center pins there are designated USB D+ and D-. The top wire connection in that diagram is +5V and the bottom wire is 0V.

    Google may have some better annotated diagrams, but the connections will be similar. Without the resistors, expect it not to work or to charge slowly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks for the answers btw, but now i need more xD, while waiting for the resistors i tried shorting the data+ and data- just by connecting the two, and the phone charged! but... not really, since the icon was there, but the percentage wasnt going up, but down xD, is this because of the resistors i need? and also, what part of the 5v boost converter do i connect my resistors to? the regulator? capacitor (assuming that's the round black thing)? xD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks for the answers btw, but now i need more xD, while waiting for the resistors i tried shorting the data+ and data- just by connecting the two, and the phone charged! but... not really, since the icon was there, but the percentage wasnt going up, but down xD, is this because of the resistors i need? and also, what part of the 5v boost converter do i connect my resistors to? the regulator? capacitor (assuming that's the round black thing)? xD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    *kinda

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    Well yeah, i Linda figured that wasnt alot, so im asking. Should i go for 3aa's? 4? And should i connect Them in series like they usually are or in parallel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    What are you powering that circuit with?

    A couple of AA batteries? It will take a long time to charge your phone if so.

    The resistors connect to the USB D+ and D- lines and to the 5V and 0V connections. In the link that Petri showed, the USB connector is shown on the right (i.e. corresponds to the USB connector on your board), and the two center pins there are designated USB D+ and D-. The top wire connection in that diagram is +5V and the bottom wire is 0V.

    Google may have some better annotated diagrams, but the connections will be similar. Without the resistors, expect it not to work or to charge slowly.