• Products and Partners
    Products and Partners
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
Member's Forum Iphone charging...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 60 replies
  • Subscribers 634 subscribers
  • Views 6079 views
  • Users 0 members are here
  • usb
  • 5vdc
  • iphone
Related

Iphone charging...

e14 Contributor
e14 Contributor over 11 years ago

Hello, my name is Martin
I have a very big problem with a 5v usb boost circuit. When i connect the circuit to the power, the led lights up, but no power... to iphones... everything else works, just not iphones. i already tried shorting the data ports with the 5v pin, AND THAT USED TO WORK, but not now!!!??

PLEASE HELP

I have now tried with adding some resistors to data+ and minus, still nothing image

 

HELP!!!

 

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    http://www.voltaicsystems.com/blog/choosing-usb-pin-voltages-for-iphones-and-ipads/

    Seems that different iphone versions behave differently. Quite picky about voltages at datalines. 2.75V D- and 2.00V D+ seems to work best.

    PS3 controller is even worse: It needs to negotiate with a host to initiate charging. I used a ATTiny45 and V-USB, but it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    i have tried 2,75, 2,8, everything now... NOTHING it still says accesory not supported! i've even tried with 2.0 v on both data + and data -, and nothing. PLEASE HELP! i initially thought this was THE ANSWER but nope, not really, still doesnt work. help... please, im losing hope here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    i have tried 2,75, 2,8, everything now... NOTHING it still says accesory not supported! i've even tried with 2.0 v on both data + and data -, and nothing. PLEASE HELP! i initially thought this was THE ANSWER but nope, not really, still doesnt work. help... please, im losing hope here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to gadget.iom

    Pin 1 voltage levels from 4.5V to 5.25V, the actual current drawn by the device varies

     

    Silicon chip ran an article (August 2013 ??) on the voltages required on both USB pins to make the various Apple products draw their full capability.

    It seems that unless the Apple device sees that voltage, it won't use the full current draw of the supplying device (ie 5v x amp supply)

     

    It was quite interesting because the ratios of resistors required was not simple.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to e14 Contributor

    Check your voltages:

    A general observation with the Apple products is that they will attempt to draw the maximum current if and only if the voltage level on Pin 1 with respect to the current draw remains constant between 5 and 5.25 volts.  Often, if a charger is unable to supply the proper amount of current the voltage output will drop.  For instance, a 5.25V 1A power supply may only output to 4.5V when under a 2A load.  For Apple products, when a device is presented with any one of the voltage configurations (500mA, 1A, or 2A) and then presented with a range of Pin 1 voltage levels from 4.5V to 5.25V, the actual current drawn by the device varies.  In our tests, we found that when the voltage sent to the iPad 2 was 4.5V, the iPad 2 drew only about 1A, but steadily scaled up the current to 2A as the voltage was incrementally increased to 5V.  Additionally, we noted Apple devices will not accept charge from power supplies with Pin 1 voltages of less than 4.5V or greater than 5.5V.

     

    Extract from Peri's link: http://www.voltaicsystems.com/blog/choosing-usb-pin-voltages-for-iphones-and-ipads/