• Products and Partners
    Products and Partners
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
Member's Forum PiFace Digital 2 rack
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 632 subscribers
  • Views 646 views
  • Users 0 members are here
  • element14
Related

PiFace Digital 2 rack

e14 Contributor
e14 Contributor over 10 years ago

Is there a rack for PiFace Digital 2, like it is for the previous model?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Rack does not exist for 40 pins, but a shim may work in it's place. PiFace PiFace Shim Module | 2445464 | PiFace

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thank you for the hint. So you think I can still use the PiRack to connect the PiFace digital2 boards via the Shim onto the PiRack and also to use Shim to connect PiRack itself to connect to raspi 40pins?

    the signals to address the correct piface board from raspi are usable by using shim and reduced 26pin set?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    The new PI Face relay boards for the PI2 are self stacking and would not need this, they also have way more relays on them, upto 8 if needed on a single board (With the relay extra) and that still leaves 8 more gpio on the 12 pin header

    Image result for piface relayImage result for piface relay

    you also need to be sure the older PFDigital boards will work on the PI2 as there where changes to the SPI bus

     

    One other thing to remember, you did not say the use. NONE of the PI face digital boards are rated for controlling mains devices (Infact anything much more than 20 or 30 V is not supported)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Thank you Peter. That sounds really interesting. I will test it out!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Thank you Peter. That sounds really interesting. I will test it out!