• Products and Partners
    Products and Partners
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
Member's Forum Help, Pi2 and MCP3008
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 631 subscribers
  • Views 1871 views
  • Users 0 members are here
  • mcp3008
  • spi
  • analog
  • pi2
Related

Help, Pi2 and MCP3008

e14 Contributor
e14 Contributor over 10 years ago

My analog board and Pi2 are inside a well ventilated metal enclosure. The MCP3008 is not getting warm to the touch. There is a fan pushing air though the enclosure.

 

All signals look clean on the scope.

 

Vcc, and Vref are 3.3v.  All samples are within 0-3.3v.

 

I have tried all different SPI clocks form 500Khz to 3Mhz.

 

An identical board sitting on my desk has been working fine for 45 min.  Three different PI and MCP3008 inside the metal enclosure will work for about 5 min after a power cycle then the readings go nuts, before all eight channels revert to zero.

 

I will leave the working board running all night.  The AC cuts off here at about now.  So the temp in this office will go up over night to about 30c (Singapore) so I guess I will know if the temperature affects it.

 

Here is my "transfer" code:

 

//==================================================================

//Private main read/write

//==================================================================

int CMCP3008::spiWriteRead( unsigned char *data, int length)

{

  struct spi_ioc_transfer spi[length];

  int i = 0;

  int result=-1;

 

    //One spi transfer for each byte

    for(i=0;i<length;i++)

    {

      memset(&spi[i],0,sizeof(spi[i]));              //Flush

      spi[i].tx_buf        = (unsigned long)(data+i); //Transmit from "data"

      spi[i].rx_buf        = (unsigned long)(data+i); //Receive into "data"

      spi[i].len           = sizeof(*(data+i));

      spi[i].delay_usecs   = 0;

      spi[i].speed_hz      = this->speed;

      spi[i].bits_per_word = this->bitsPerWord;

      spi[i].cs_change = 0;

    }

 

    result=ioctl (this->spifd,SPI_IOC_MESSAGE(length),&spi) ;

    if(result<0) {  printf("spiWR==[%i]\n",result); return -1; }

 

  return 0; //Success

}

 

Please help

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Your code is a bit odd, you only need one of those structs, not an array surely?

    A single struct is sufficient to transfer multiple bytes, since the rx_buf and tx_buf are arrays.

    Anyway, although incorrect it looks benign, it shouldn't cause issues.

    I personally don't use the same locations for rx and tx, whereas you have them both

    pointing to the data array. If it doesn't cause an issue then great - it's just something I've never

    done. and I've never tested to see if it is possible.

    Apart from that I can't see an issue with the code but I've only examined it briefly.

    I think you're saying the MCP and Pi are in the same enclosure. Do you have anything like long cables from the

    MCP to the sensor? Perhaps you're getting noise on them?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thank you.  I have been so frustrated that I overlooked the "oddity".  but as you said, it is not likely to be the problem.  The device on my desk has a longer cable run than the device in the enclosure. The readings are dead on.

     

    This is the rest of my object:

     

    //==================================================================

    //Read

    //==================================================================

    float CMCP3008::readADC(int Channel)

    {

        unsigned int  read;

        float value;

        float result=0;

        float m_Step=.003222656;

     

        //Read value

        read=analogRead(Channel);

        value=(float)read;

        result=value*m_Step;

     

        return result;

    }

     

    //==================================================================

    //Read with Multiplier

    //==================================================================

    float CMCP3008::readADC(int Channel,int Mult)

    {

        float value;

        float mult=(float)Mult;

     

        value=readADC(Channel);

     

        if(Mult==1) return value;

        return value*mult;

    }

     

    //==================================================================

    //Constructor

    //==================================================================

    CMCP3008::CMCP3008()

    {

        this->mode=SPI_MODE_0;

        this->bitsPerWord=8;

        this->speed=1000000;     //Default to one MHz

        this->spifd=-1;

    }

     

    //==================================================================

    //Destructor

    //==================================================================

    CMCP3008::~CMCP3008()

    {

        this->spiClose();

    }

     

    //==================================================================

    //Private Raw read (with averaging)

    //==================================================================

    //Do six reads

    //Drop the one highest, and one lowest

    //Average the remaining 4

    unsigned int CMCP3008::readAverage(int Channel)

    {

        unsigned int read;

        unsigned int result=0;

        unsigned int highest=0;

        unsigned int lowest=0x3FF;

        int cnt=0;

     

     

        analogRead(Channel);    //Dummy read

        while(cnt<5)        //Do six reads

        {

            read=analogRead(Channel);

            if(read>highest) highest=read;    //If highest

            if(read<lowest)  lowest=read;    //If lowest

            result+=read;

            cnt++;

        }

        result-=highest;    //Remove the highest

        result-=lowest;        //Remove the lowest

        result>>=2;        //div by 4

        result&=0x3FF;        //Bounds

     

        return result;

    }

     

    //==================================================================

    //Private raw read

    //==================================================================

    unsigned int CMCP3008::analogRead(int Channel)

    {

        unsigned int a2dVal=0;

        unsigned char data[3];

        unsigned char config;

        int result=0;

     

         data[0]=0b00000001;          //First byte transmitted -> start bit

        Channel&=7;            //Mask off any rouge illegal values

        config=(unsigned char)Channel;    //Get the channel

        config|=8;            //Single ended operation

        config<<=4;            //Move the three bits over

        data[1]=config;

        data[2]=0b00000000;         //Third byte transmitted....don't care (zero)

     

        //Do the transactions

        result=this->spiWriteRead(data,3);

        if(result<0) return 0;

     

        //Ignore data[0]

        a2dVal=(unsigned int)(data[1]&0x03);    //Lowest two bits of data[1]

        a2dVal<<=8;                //Position for merge

        a2dVal|=(unsigned int)data[2];        //All eight bits of data[2]

        a2dVal&=0x3FF;                //Mask

     

        return a2dVal;

    }

     

    //==================================================================

    //Private main read/write

    //==================================================================

    int CMCP3008::spiWriteRead( unsigned char *data, int length)

    {

     

      struct spi_ioc_transfer spi[length];

      int i = 0;

      int result=-1;

     

        //One spi transfer for each byte

        for(i=0;i<length;i++)

        {

          memset(&spi[i],0,sizeof(spi[i]));              //Flush

          spi[i].tx_buf        = (unsigned long)(data+i); //Transmit from "data"

          spi[i].rx_buf        = (unsigned long)(data+i); //Receive into "data"

          spi[i].len           = sizeof(*(data+i));

          spi[i].delay_usecs   = 0;

          spi[i].speed_hz      = this->speed;

          spi[i].bits_per_word = this->bitsPerWord;

          spi[i].cs_change = 0;

        }

     

        result=ioctl (this->spifd,SPI_IOC_MESSAGE(length),&spi) ;

        if(result<0) {  printf("spiWR==[%i]\n",result); return -1; }

     

      return 0; //Success

    }

     

     

    //==================================================================

    //SPI open

    /Added SPI clock setting

    //==================================================================

    int CMCP3008::spiOpen(std::string devspi,unsigned int Speed)

    {

        int result=0;

     

        //Set Speed

        this->speed=Speed;

     

        //Open

        this->spifd = open(devspi.c_str(), O_RDWR);

        if(this->spifd<0) result=-1;

     

        //Set SPI write mode

        if(result==0)

        {

            result=ioctl (this->spifd, SPI_IOC_WR_MODE, &(this->mode));

            if(result<0) result=-1;

        }

        //Set SPI read mode

        if(result==0)

        {

            result = ioctl (this->spifd, SPI_IOC_RD_MODE, &(this->mode));

            if(result<0) result=-1;

        }

        //Set bits per word for write

        if(result==0)

        {

        result = ioctl (this->spifd, SPI_IOC_WR_BITS_PER_WORD, &(this->bitsPerWord));

            if(result<0) result=-1;

        }

        //Set bits per word for read

        if(result==0)

        {

            result = ioctl (this->spifd, SPI_IOC_RD_BITS_PER_WORD, &(this->bitsPerWord));

            if(result<0) result=-1;

        }

        //Set write speed

        if(result==0)

        {

            result = ioctl (this->spifd, SPI_IOC_WR_MAX_SPEED_HZ, &(this->speed));

            if(result<0) result=-1;

        }

        //Set read speed

        if(result==0)

        {

           result = ioctl (this->spifd, SPI_IOC_RD_MAX_SPEED_HZ, &(this->speed));

            if(result<0) result=-1;

        }

     

        if(result)     { printf("MCP3008 (%s) open failed!\x0A\x0D",devspi.c_str()); return -1; }

     

        printf("MCP3008 (%s) Open\x0A\x0D",devspi.c_str());

        return 0;    //Success

    }

     

    //==================================================================

    //Private SPI close

    //==================================================================

    int CMCP3008::spiClose()

    {

        int result=-1;

     

        result=close(this->spifd);

     

        if(result< 0)  result=-1;

        else result=0;

     

        return result;

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    If the code works on your desk but not in the real environment, it is likely to be an electronic/electrical issue.

    The environment can have an effect.

    How long are the cables to the sensor, and what is the sensor? Probably some photo is needed showing in detail your arrangement, cables and sensor and the boards.

    Does the MCP3008 board have any input buffering? Most cheap ADC boards neglect this, and as a result can cause issues with incorrect readings. I've noticed the code eliminates two readings from six and then averages the remainder; was this because you're getting very noisy readings?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    IT WORKS!

     

    I added some op amps as voltage followers.  On the input side I set up pi filters to create a super low pass filter.( 4.7uF, 1mH, 1uF ) and a resistor to ground to discharge the 4.7uF cap.  On the output of the op amps  I used 330 ohm resistors and 1uF caps.

    The values read are dead on!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    It appears to be dropping into low power mode and staying there. 

     

    I do not understand it, because the readings are accurate to three decimal places.

     

    I will isolate the inputs. I am having the boards redone with low power op amps as voltage followers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    It appears to be dropping into low power mode and staying there. 

     

    I do not understand it, because the readings are accurate to three decimal places.

     

    I will isolate the inputs. I am having the boards redone with low power op amps as voltage followers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    IT WORKS!

     

    I added some op amps as voltage followers.  On the input side I set up pi filters to create a super low pass filter.( 4.7uF, 1mH, 1uF ) and a resistor to ground to discharge the 4.7uF cap.  On the output of the op amps  I used 330 ohm resistors and 1uF caps.

    The values read are dead on!