Member's Forum TIP120 Transistor for AC voltage?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 9 answers
  • Subscribers 631 subscribers
  • Views 3339 views
  • Users 0 members are here
  • valve
  • transistor
  • ac
  • sprinkler
Related

TIP120 Transistor for AC voltage?

ntewinkel
ntewinkel over 10 years ago

Hello all!

 

My sprinkler controller is starting to act up and it's so old I can't find replacement parts!

 

So I'm thinking of using a Raspberry Pi to control the valves. I've noticed online opensprinkler.com has done this before. I like their setup, and might also buy their solution, but being a DIY Maker type I'd like to also try this myself.

 

The very first thing I noticed is that the valves are all made to run on 24v AC. The old sprinkler controller has a 24v AC adapter.

 

I have TIP120 transistors, but I can't tell by the datasheet if it can be used to switch AC voltages.

 

I also have TOP223Y transistors, which do state that they can switch AC.

 

Or if you have any other ideas that might be more suitable, that would also be welcomed advice!

 

What do you think?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
  • dougw
    0 dougw over 10 years ago in reply to ntewinkel

    I was looking for cheaper devices as well, but I only had to buy 3. I might go with the MOC solution if I have a large number to implement.

    The Vishay BRT1x series might be a bit cheaper.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to ntewinkel

    I used Vishay VO2223A in the Henrietta Project Furnace Interface.

    They cost about $2 and switch about 1 amp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to ntewinkel

    ps, I just read more of your Henrietta project, and I see you used VO2223A chips... but from what I can find they're a bit pricey, especially when multiplied by 16 zones. dang.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to dougw

    You could use optically isolated triacs...

     

    Hi Douglas, do you happen to know of any triacs that are optically isolated and also can handle the required load: 500mA (short pulse, probably < 0.1 second) and 250mA steady (15 minutes) ?

     

    I've been looking, but the ones I found are either in the range of $5 each, or affordable and either not high enough amps, or not optoisolated.

     

    I suppose I could buy those BTA as well as MOC ones, which then comes to about 50 cents per zone (about 25 cents per chip).

     

    Many Thanks!

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago in reply to ntewinkel

    Your moc30x0 opto TRIAC usually drives another external TRIAC

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to ntewinkel

    I'm having trouble interpreting the datasheets, but it looks like the BTA family might work.

     

    From OpenSprinkler: "...the electrical properties of 24V AC solenoids. They generally require a high impulse (in-rush) current to get energized (often as high as 300 to 500mA), then they will stay on with a relatively low stable (holding) current (e.g. 150 to 250mA). "

     

    So to me it looks like it would need to (at a minimum) handle peak of 500mA and steady 250mA.

     

    If I'm reading the BTA12 datasheet correctly, it can handle 12A steady, 105 Peak, while the MOC3020 series looks like it only handles 100mA steady (and just over 1A peak).

     

    Am I reading that correctly?

     

    There tend to be lots to choose from, but I was looking at these datasheets:

    http://www.onsemi.com/pub_link/Collateral/BTA12-600BW3-D.PDF

    http://www.ti.com/lit/ds/symlink/moc3022.pdf

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to D_Hersey

    Thanks Don!

     

    I didn't know about TRIACs, but that looks like the easiest solution, as well as cost-effective (I just saw some MOC 3021s at 25 cents each on eBay, though the output current rating for those specific ones might be too low).

     

    Why wouldn't I use Triacs over the bigger relay option?

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to D_Hersey

    Y'know you can switch AC with a MOSFET if you have a supervoltage.

     

    I could try bypassing the step-down transformer on the pole by the road...
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago

    Thanks, everyone, for all the great ideas!

     

    For some reason I had not even considered using one of those pre-built relay boards, but that would be an easy solution. Relays tend to be big though, and I have seen images of the OpenSprinkler boards that show tiny components switching the valves. But even relays would be much smaller than what's currently in there.

     

    I noticed that OpenSprinkler has a blog, and they mention this:

    "OpenSprinkler v2.3 AC uses 24V AC transformer (sold separately), and triacs to drive sprinkler solenoids. OpenSprinkler v2.3 DC uses 9V DC transformer (included in the package), and MOSFETs to drive solenoids."

     

    So they use triacs.

     

    And I'm very curious about their 9v solution! He discusses a fair bit of detail about how the valves work, and apparently he's able to switch them on using a burst of voltage and current but then keeping them on with much lower current.

    "...produce a high in-rush voltage to ensure the solenoids are solidly energized, and then reduce the voltage down to produce a relatively low (150 to 250mA) holding current. According to my calculation, 9V DC is ideal for providing the required holding current. On top of that, we just need a boost converter to generate a high in-rush voltage (18~22V) required to energize the solenoids."

     

    This is all very interesting stuff image

     

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to D_Hersey

    You can use a transformer to generate your 24VAC.

     

    I was planning on using the one that's on the existing controller to bring in 24 volts to pass along to the valves. Or were you thinking of somehow generating the 24v AC from a lower voltage? ie, powering everything with a tablet USB adapter?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>