• Products and Partners
    Products and Partners
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
Member's Forum Got Any Cool Hacks for an Old Laptop?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 4 answers
  • Subscribers 634 subscribers
  • Views 3157 views
  • Users 0 members are here
  • hack
  • computer
  • repair
  • laptop
Related

Got Any Cool Hacks for an Old Laptop?

spannerspencer
spannerspencer over 10 years ago

So, I have an old laptop that's not working any more. I suspect it's the hard drive that's playing up, but the hardware was already out of date enough that it was a sluggish beast anyhow. And the battery's pretty much useless now, too.

 

I'd considered putting a new hard drive in it, and installing one brand or another of Linux on it, or possibly sidestepping the hard drive altogether and running Chromium OS from an SD card.

 

But I don't really have a particular use for a non-portable laptop even if I did these things. I've got more computers than I can use already.

 

Neither do I want to throw it away, because that's just not cricket either. All that lovely hardware must have other uses, right?

 

So I was thinking you guys might have some devilishly cunning projects, hacks, or alternative uses for the laptop, or some combination of its parts.

 

Hit me!

  • Sign in to reply
  • Cancel
  • electrorubixtech
    0 electrorubixtech over 10 years ago in reply to electrorubixtech

    Or a second display for a laptop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electrorubixtech
    0 electrorubixtech over 10 years ago

    You can make a portable monitor for raspberry pi at an laptop I don't try that yet but there is some tutorials on YouTube and my favorite video is by GreatScott! Reuse old laptop screen search this on you tube I hope you found it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • oksbwn
    0 oksbwn over 10 years ago

    You can use your old Laptop for networking stuffs like a server or Router or a firewall.....Again it depends on the requirement.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • domdv77
    0 domdv77 over 10 years ago

    I've just hacked and re-purposed the LCD screen out of a dying laptop, and it was really quite an easy process. First of all remove the actual LCD panel from the laptop lid. This may be either held in place by screws, glue or locking plastic parts. Here you can be brutal since you will be discarding the casings anyway, but be careful not to damage the LCD. Once it is free, carefully remove all the connections too as you will need these later, and look on the back for a label which will show you the model number of the LCD. I googled my serial number and found a chinese distributor selling an LCD controller board for my LCD. £19 and 8 days later, I hooked up the controller board, powered it via a universal brick adaptor for the output I needed, which was 12v 4A. Connected up a RPi2 with debian wheezy installed, and hey presto it worked. I now have an extra display to play with. this video shows everything connected and working

    https://youtu.be/jspCGCGPmww

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 10 years ago in reply to shabaz

    This is good stuff. I'd been wondering about how to at least make use of it as a screen, or for some basic "always on" function.

     

    I did see a good kitchen hack, where an old laptop was mounted upside down underneath a cabinet, so the screen swung down when you opened it. That could work nicely in a garage or workshop, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 10 years ago in reply to dougw

    Man, I LOVED my Amiga. I could start playing Speedball 2, Rocket Ranger, Populous, and Lords of the Rising Sun on it again...

     

    Noice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Hi Spanner!

     

    If it were me, I'd stick it in a garage, with a music player, and a notepad app and calculator, i.e. just the basics with most Linux desktop installs. Mainly because I always find myself needing a calculator and pen and notepad when DIY'ing, and music would be good too!

    Large text so it can be referred to from a distance, and a clock to see how much time is being wasted..

    To be honest I'm surprised no-one has created a shed distro..

    Also the Pi + capacitive display might be good for this, stuck on a wall to save space.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago

    One way to speed up operation of an old computer is to get Amiga OS running on it.

    Amiga OS runs much, much faster than Linux - even when running under Linux.

    Your machine might run AROS, icaros or AEROS.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 10 years ago

    Hi Spanner,

     

    I have a fairly old laptop, preCDRom or USB or even ethernet.

     

    What I still like about it is that it has a terminal mode so that I can use it to communicate serially with MCU's.

     

    Yes it is slow, but it will run 9600 baud, which is enough for most applications.

     

    Given the lack of serial ports on newer laptops, it makes a nice smart terminal.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Once upon a time, around the mid of 1980s, there was in Turin a very strange nighty bar. All the seats was by wooden and aluminium from an old tram and a lot of old computer monitors sealed and filled with water and nice coloured fishes.

     

    I'd like to make a water-fish screen replacing the broken screen of an old laptop over it I will install a headless os and connect it with a Raspi for some external controls, sensors etc.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>