Member's Forum Interfacing generic power banks with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 629 subscribers
  • Views 257 views
  • Users 0 members are here
Related

Interfacing generic power banks with Arduino

pathfider1998
pathfider1998 over 10 years ago

So I have a project where I am designing battery powered spotlights (not a work light, those gooseneck lamps you can freely position to wherever you want) using cheap single-cell power banks, wireless charging docks and generic gooseneck ceiling lamp fitting.

Because I cannot use Xiaomi power banks (which are high capacity, automatically switched, has charge-while-using function and so on) because I have to keep the weight, size and cost to the minimum (while not making the entire contraption fly into stratosphere), I have to switch the power banks almost manually. (some power banks DO switch on when there's load, by the way)

Since I am groundless in this field, I am asking you people to help me a little bit.

 

Planned features:

  • Sense light
  • Turn off LED when the light level reaches certain level
  • Either use fixed PWM (about 30%) or a slowly decreasing PWM (60~20%) to preserve power, probably in 10% step to simplify?
  • Enter low-power mode after 5 minutes of LED turning off
  • Use wireless charging pads (like Qi branded generic ones?) and a classic-looking stick-and-a-hook type device to charge
  • 1W warm-white LED

 

Pseudo-code (bad code, I know) :

See if room is dark

If room is dark

     If power bank is on

          Press and hold button for few seconds

          Turn on the LED

     Else

     Press and hold button for few seconds

     Turn on the LED

Else

     Turn off the LED

     If power bank is on

          Press and hold button for few seconds

     Else

          Return