• Products and Partners
    Products and Partners
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
Member's Forum New Member & Can RPi Zero Control Stepper Motors Query
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 6 answers
  • Subscribers 633 subscribers
  • Views 2183 views
  • Users 0 members are here
  • bipolar stepper motor
  • new_member_introduction
  • pi zero
Related

New Member & Can RPi Zero Control Stepper Motors Query

drmac
drmac over 10 years ago

Just joined, hello all.

I joined to help learn about controlling stepper motors for a few little projects I'm working on. One query is whether or not the RPi Zero can also be used to run stepper motors as out lined for example in TUTORIAL - How to control a bipoloar 4 wire stepper motor? I've not come across anything about the zero doing so. If there is info out there I would appreciate a pointer or two


 

Cheers,


 

Niel


 

  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 9 years ago

    I agree with Peter.

     

    The main thing you have to keep in mind is that the IO pins on the PI Zero can only source so much current.

     

    So to properly drive stepper motors you want to put either a motor controller between them or add driver transistors on a separate power buss to ensure that you do not overtax the PI Zero, or any other processor, IO capabilities.

     

    The devil is in the details, so you need to look at the current drive requirements of the motors, and the control card.

     

    As long as you do not violate those limits, you can drive a lot of different devices with any MCU, but you need to take care or you release the magic smoke.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • drmac
    0 drmac over 9 years ago in reply to DAB

    DAB

     

    Understood, thanks for the info, However I can't find the stepper motor (OKI EM-546 12V with 48 steps per revolution) datasheet so any suggestion regards measuring the motor drive current?

     

    Cheers,

    Niel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to drmac

    Use Ohms law V=IR (voltage = current x resistance). The sum can be reconfigured to I=V/R (Current = Voltage divided by Resistance).

     

    You know the voltage is 12V right so you have 1 piece of information, the next part is to find the resistance of the coils. Bipolar stepper motors have 4 wires, you'll find that they are connected in pairs to a coil within the stepper motor. Measure each pair with a multimeter on Ohm's or resistance setting (each pairs result should be the same) and apply the sum above to your value so Current=12/ohm's

     

    (another useful piece of information is that stepper motors can be used at a greater voltage by reducing the current proportionally, this helps with overcoming back emf and energising each coil phase faster resulting in increased performance but is probably getting out of the scope of somebody just approaching stepper motors).

     

    Hope this helps and good luck!!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to drmac

    Use Ohms law V=IR (voltage = current x resistance). The sum can be reconfigured to I=V/R (Current = Voltage divided by Resistance).

     

    You know the voltage is 12V right so you have 1 piece of information, the next part is to find the resistance of the coils. Bipolar stepper motors have 4 wires, you'll find that they are connected in pairs to a coil within the stepper motor. Measure each pair with a multimeter on Ohm's or resistance setting (each pairs result should be the same) and apply the sum above to your value so Current=12/ohm's

     

    (another useful piece of information is that stepper motors can be used at a greater voltage by reducing the current proportionally, this helps with overcoming back emf and energising each coil phase faster resulting in increased performance but is probably getting out of the scope of somebody just approaching stepper motors).

     

    Hope this helps and good luck!!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • DAB
    0 DAB over 9 years ago in reply to e14 Contributor

    You also need to assess the coil reactance, not just the wire resistance.

     

    You get different effects with frequency and stray capacitance in the leads.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer