• Products and Partners
    Products and Partners
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
Member's Forum N64 Portable (Please Help) continued
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 631 subscribers
  • Views 2181 views
  • Users 0 members are here
Related

N64 Portable (Please Help) continued

adamsoileau1
adamsoileau1 over 8 years ago

Thank you to everyone on my last question, I used 12 volts instead of 8, and the converter worked and the red light on the n64 was on. But the N64 was not booting. This also happened when I was experimented with another power source, where the red Light would be on, but that is it. I re wired the original power connector and it worked perfectly. Any tips? I have tried to run 8.4 volts at 6000mah and I also tried it at 12 volts at 3000mah, both did not boot, (but the light was on)

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Adam,

     

    According to the photo here:

    How to test the N64 AC power adapter with a voltmeter

    the Nintendo 64 needs 12V at up to 800mA worst case, and 3.3V at up to 2.7A. That will require a pretty good DC-DC converter, and will also require you to supply 12V as well, not 8.4V.

    What DC-DC converter are you using, and what battery are you using to supply 12V? If you have links to them then that would help.

     

    Also, to debug this, do you have a multimeter? If not, you really need one (cheap ones are $5, if you intend to do more than just this project then better ones are listed here Deck The Bench - Engineer Wish List  , but a $5 one will be fine). Then, you can check the voltages (12V and 3.3V) on the power source and DC-DC converter _before_ it is plugged into the Nintendo 64, and then you can re-check after it is connected to the Nintendo 64 to see if the rails are sagging (due to battery choice or DC-DC converter issues).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • adamsoileau1
    0 adamsoileau1 over 8 years ago in reply to shabaz

    I have ordered this boost converter to get 12 volts. That, or I could use 6 1850 batteries. In series and parallel. Do you recommend one or the other?

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • adamsoileau1
    0 adamsoileau1 over 8 years ago in reply to shabaz

    I have ordered this boost converter to get 12 volts. That, or I could use 6 1850 batteries. In series and parallel. Do you recommend one or the other?

    Attachments: