• Products and Partners
    Products and Partners
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
Member's Forum N64 Portable (Please Help) continued
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 631 subscribers
  • Views 2181 views
  • Users 0 members are here
Related

N64 Portable (Please Help) continued

adamsoileau1
adamsoileau1 over 8 years ago

Thank you to everyone on my last question, I used 12 volts instead of 8, and the converter worked and the red light on the n64 was on. But the N64 was not booting. This also happened when I was experimented with another power source, where the red Light would be on, but that is it. I re wired the original power connector and it worked perfectly. Any tips? I have tried to run 8.4 volts at 6000mah and I also tried it at 12 volts at 3000mah, both did not boot, (but the light was on)

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Adam,

     

    According to the photo here:

    How to test the N64 AC power adapter with a voltmeter

    the Nintendo 64 needs 12V at up to 800mA worst case, and 3.3V at up to 2.7A. That will require a pretty good DC-DC converter, and will also require you to supply 12V as well, not 8.4V.

    What DC-DC converter are you using, and what battery are you using to supply 12V? If you have links to them then that would help.

     

    Also, to debug this, do you have a multimeter? If not, you really need one (cheap ones are $5, if you intend to do more than just this project then better ones are listed here Deck The Bench - Engineer Wish List  , but a $5 one will be fine). Then, you can check the voltages (12V and 3.3V) on the power source and DC-DC converter _before_ it is plugged into the Nintendo 64, and then you can re-check after it is connected to the Nintendo 64 to see if the rails are sagging (due to battery choice or DC-DC converter issues).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • adamsoileau1
    0 adamsoileau1 over 8 years ago in reply to shabaz

    I do have a multi meter. I am using 4 1850 batteries. In parallel and series, so 7.4-8.4 volts with double the amps. The 12 volts, I was testing with a plug adapter, 12 volts at 3000mah. I am using a Texas Instruments WAS chip to get 3.3 volts. I hope to get a knew one that runs on 7.4 volts and not 12 volts. WAS PTH08080.

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to adamsoileau1

    What voltage do you measure from the output of the boost converter, and from the output of the TI module?

    Do the voltages change when you connect them to the N64 and power it up? If so, what voltages do you measure? Does it fluctuate?

    Without this information, it is all guesses.

    The information is needed to a couple of decimal places by the way, because it is not known what multimeter accuracy you have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago in reply to adamsoileau1

    What voltage do you measure from the output of the boost converter, and from the output of the TI module?

    Do the voltages change when you connect them to the N64 and power it up? If so, what voltages do you measure? Does it fluctuate?

    Without this information, it is all guesses.

    The information is needed to a couple of decimal places by the way, because it is not known what multimeter accuracy you have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to adamsoileau1

    Kind-of clutching at straws here. If you don't supply enough information, you can't expect sufficient information in return.

    If you're supplying the correct voltages to the correct pins, it should work.

    It really is up to you to measure and confirm both voltages, and the pinout, or at least show the connections in detailed photographs if you've already measured the voltages.

    And if you have measured and confirmed them before you seeked help, then you ought to have mentioned it, to save this back-and-forth of messages.

     

    I've already asked for you to measure both voltages, and I don't really want to nag and ask you again.

    There is only finite time I can spend on a problem, it really is a waste, I could have helped more if I'd had more information. I'm finished for the evening.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • adamsoileau1
    0 adamsoileau1 over 8 years ago in reply to shabaz

    Also do you recommend a better way to power the n64 off of 18650 batterries?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adamsoileau1
    0 adamsoileau1 over 8 years ago in reply to shabaz

    It stays at 3.4 volts connected or not. My multi meter is known to wrong at most by two tenths.