• Products and Partners
    Products and Partners
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
Member's Forum How to connect USB/Ethernet shield?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 631 subscribers
  • Views 587 views
  • Users 0 members are here
  • diode
  • usb
  • shield
  • lm317
Related

How to connect USB/Ethernet shield?

mpiechotka
mpiechotka over 8 years ago

I'm slowly finalizing my first, toy, design and I'm almost ready to send it for production. I have two outstanding questions:

 

a) I don't know what should I connect shield of USB port to. It seems that recommended way is to connect to metal chassis (which I don't have). I connected it to holes in PCB (which would connect to non-existing chassis) and put 2 0.1 µF and 10 kΩ resistor to the ground (in parallel) but I'm not sure if this is correct way.

 

b) I power the design out of either of 2 USB ports I have. I put diodes between LM317 and each VBUS but I could not find any diodes which would have low forward voltage drop (<1.7 V) and was rated for peak currents (300 mA based on the characteristic). I presume diodes have too much differences between each other to put two in parallel with lower rating as one might have slightly lower voltage drop and take most current. Am I missing some keywords for diodes I should search for or should I put a different type of voltage regulator? I don't know what exactly I did wrong but I started being able to find such diodes.

 

image

imageimage

  • Sign in to reply
  • Cancel
  • mpiechotka
    0 mpiechotka over 8 years ago in reply to DAB

    I added the schematics. D1 and D2 are diodes I was asking about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago

    Can you provide some pictures and circuit diagrams?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer