• Products and Partners
    Products and Partners
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
Member's Forum Old analogue monitor help?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 631 subscribers
  • Views 1960 views
  • Users 0 members are here
  • esp32
  • wifi
  • monitor
  • monochrome
  • esp8266
  • crt
  • art
Related

Old analogue monitor help?

frozr
frozr over 8 years ago

Hi all,

 

I live in the UK. We have a gambling chain here called 'Coral'. One day my friend dragged me in and I got to see that there was a little CRT looking TV. I asked if it's still in use and learned that it's been there for quite a while. I ended up getting it, absolutely free of charge. It even came with a keyboard (made of original Cherry switches from the 90s!). I've learned as much as I could about it and learned that it seems to be nothing more than some sort of generic monochome monitor, with what seems some sort of old microcontroller which is actually used to display the betting tables on the monitor screen and take input from the keyboard. They aren't particularly valuable (not that I'd want to sell it), so I want to convert it into maybe something using the ESP32 or preferably ESP8266, since I've a few of those laying around. I know CNLohr on youtube did an interesting video on how capable the ESP8266 is (https://www.youtube.com/watch?v=SSiRkpgwVKY ).  However; I need help with understanding how I can display on the monitor. I've very little understanding of analogue electronics, a vague understanding of digital electronics and mediocre programming skills. I really don't know who to turn to other than this forum.

 

Here's the board that seems to actually have control of what's on the screen.

This is seemingly the only digital board within the monitor. The 'missing chip' is actually something truly special. The creators (OTT Keyboards) used that socket, and what looks like an IDE cable to go between the board and whatever is on the outside. The IDE cable also connected to something that looks like an old serial port? Not sure.

 

Only cables between the board and the monitor.

These are the only cables between the board and the monitor. Each cable consists of 3 smaller cables, of the same colour set. In the background you can also see a piezzo speaker, and yes, that tape was used to stick it to the outside case of the monitor.

 

The two cables disappearing under the CRT itself.

 

The two cables from the PCB disappearing under the CRT itself.

 

Below are some more detailed shots of the PCB for anyone interested in helping out or interested in some almost hand made electronics.

 

image

image

In the pictures above, you can see the very odd IDE cable solution actually being strapped down with a zip tie. Also notice how much it sticks out.

 

image

Another closeup shot of the ICs.

 

image

Here's what was actually accessible from the back of the monitor. This is what was connected via that IDE looking cable into the empty socket on the PCB.

 

What I know so far:

 

-The ST M27C1001-12F1 is an EEPROM IC, so from what I know that's simply where the program is stored. This could be entirely wrong, but it could make sense since when pulled out, the monitor displays squares and squiggles. It's a checkered pattern, but doesn't display anything. Datasheet: https://www.mouser.co.uk/datasheet/2/389/stmicroelectronics_cd00000511-1204383.pdf

-The Toshiba TC5517CPL-20 is from what I understand RAM.

Datasheet: TOSHIBA - datasheet pdf

-NEC D43256BCZ-70LL is in the category of 'SRAM' on usbid.com.

Datasheet: https://www.usbid.com/assets/datasheets/91/d43256bcz70ll.pdf

-With the yellow dot sticker, we have a Motorola MC6847P. Wikipedia abbreviated it to 'Motorola 6847', whilst saying it's a video display generator. I can assume what it does but I understand fairly little about it.

Datasheet: https://www.datasheets360.com/pdf/1867023960849380503

Wikipedia: https://en.wikipedia.org/wiki/Motorola_6847

-2 chips labeled 74HCT365N. According to digikey.be they're buffers. I assume they're video buffers of some sort?

Datasheet: https://media.digikey.com/pdf/Data%20Sheets/NXP%20PDFs/74HC(T)365_Rev3.pdf

-74HCT00N. I found something about it being NAND? As in NAND flash I'd assume? Not really sure.

Datasheet: https://www.mouser.co.uk/datasheet/2/916/74HC_HCT00-1318972.pdf

-R65C02P2 is apparently a microprocessor working at 2MHz which "for some reason found its way into many thousands of Gotleib pinball machines." according to silicon-ark.co.uk

Datasheet: https://www.silicon-ark.co.uk/datasheets/R65c02p2-datasheet-rockwell.pdf

-R65C21P1 I found that it is a PIA (Peripheral Interface Adapter). I assume this is for interaction with the keyboard that came with the monitor.

Datasheet: https://www.alldatasheet.com/datasheet-pdf/pdf/128134/ETC1/R65C21P1.html

-74HCT139N is a demultiplexer.

Datasheet: http://www.mouser.com/ds/2/302/74HC_HCT139-351015.pdf

-SN74LS74AN contains 2 independent D type positive-edge-triggered flipflops. This tells me a little as a noobie, I understand what it is but can't exactly imagine what it'd be used for.

Datasheet: http://www.ti.com/lit/ds/symlink/sn74ls74a.pdf

-SN74LS04N is listed as an inverter. Not sure what it inverts though. Signals? 0 into 1s and vice versa?

Datasheet: http://www.ti.com/lit/ds/symlink/sn74ls04.pdf

-CD74HCT245E is listed as Bus Transceivers. I can just about manage to understand what that does.

Datasheet: http://www.ti.com/lit/ds/symlink/cd74hct245.pdf

 

I think that's all of them covered. Judging by what these ICs are listed as, it lead me to understand that what that whole board is a simple computer the likes of the 80's computers (ZX Spectrum, Commodore etc.). This leads me to believe that something as the aforementioned ESP8266 could do the job of the whole PCB just fine. I would love some help with making this into a somewhat interactive little CRT with the ability to run simple visual sketches the likes of some simple Javascript animation, as without help I physically have no idea where to go.

 

Thanks,

J.

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    0 jc2048 over 8 years ago

    I agree with MK. If it were me, I'd do something with the original processor since it's all there and presumably working. I doubt you'd have too much of a problem finding a cross-assembler that you could use. You'd need a way to erase the EPROM (UV light in an eraser box) and reprogram it (programmer) (read the contents and save it to a file before you erase it the first time). (Note, it's not an EEPROM, but if you could find an EEPROM with the same pin-out and similar specs it might be easier to work with than the EPROM - you'd just need the programmer then).

    Otherwise you could either replace it entirely and have the design job of getting a microcontroller to generate video waveforms (not as easy as you might think, unless you just copy something that someone else has got working, if there is such a thing) or you could try and find a way to interface a microcontroller to the 6847 (quite messy, but might be possible). Some of this depends on what you want from it. If you just want a terminal to use, I'd say work with the original or substitute something that's already been done. If you want a microcontroller project to learn with, weigh up the various approaches and decide which interests you, what you feel you might be capable of, and whether you have suitable equipment to do it (oscilloscope, for instance) .

     

    Display interface is a 6847. Bit later than the 6845 - has more integrated on the chip - internal character ROM and puts out Y (luminance)  and colour-difference signals.

     

    Possible that the output might be composite - the two transistors on the left look like they might be a circuit for combining the HS and VS with the Y output. Find pin 12 (Y output - that's the luminance signal) of the 6847 and trace where it goes (you might need to carefully lift the chip out of its socket to see tracks underneath). Also trace the HS and VS outputs. Draw the circuit as you go and you'll then have a diagram of the video output stuff and know how it drives the monitor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 8 years ago

    I agree with MK. If it were me, I'd do something with the original processor since it's all there and presumably working. I doubt you'd have too much of a problem finding a cross-assembler that you could use. You'd need a way to erase the EPROM (UV light in an eraser box) and reprogram it (programmer) (read the contents and save it to a file before you erase it the first time). (Note, it's not an EEPROM, but if you could find an EEPROM with the same pin-out and similar specs it might be easier to work with than the EPROM - you'd just need the programmer then).

    Otherwise you could either replace it entirely and have the design job of getting a microcontroller to generate video waveforms (not as easy as you might think, unless you just copy something that someone else has got working, if there is such a thing) or you could try and find a way to interface a microcontroller to the 6847 (quite messy, but might be possible). Some of this depends on what you want from it. If you just want a terminal to use, I'd say work with the original or substitute something that's already been done. If you want a microcontroller project to learn with, weigh up the various approaches and decide which interests you, what you feel you might be capable of, and whether you have suitable equipment to do it (oscilloscope, for instance) .

     

    Display interface is a 6847. Bit later than the 6845 - has more integrated on the chip - internal character ROM and puts out Y (luminance)  and colour-difference signals.

     

    Possible that the output might be composite - the two transistors on the left look like they might be a circuit for combining the HS and VS with the Y output. Find pin 12 (Y output - that's the luminance signal) of the 6847 and trace where it goes (you might need to carefully lift the chip out of its socket to see tracks underneath). Also trace the HS and VS outputs. Draw the circuit as you go and you'll then have a diagram of the video output stuff and know how it drives the monitor.