• Products and Partners
    Products and Partners
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
Member's Forum Paranormal Sensor Suggestions?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 9 answers
  • Subscribers 634 subscribers
  • Views 3605 views
  • Users 0 members are here
  • raspberry pi
  • ghosts
Related

Paranormal Sensor Suggestions?

Sean_Miller
Sean_Miller over 7 years ago

I had a couple of ambitious true ghost hunters approach me about a build to help them on their adventures.

 

I'm definitely going to help them with a raspberry pi solution.  However, I feel like I could use some more sensors.  Here's what I thought of so far:

 

  • Temperature (if it changes a degree in less than 10 seconds)
  • PIR motion sensor
  • Infrared camera that records
  • Record audio
  • Voltage sensing poles (thinking I would just have some metal rods that would allow me to detect a change in voltage between the two.

 

 

What other thoughts do you have that would be cool for ghost hunting?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    0 14rhb over 7 years ago

    Coincidentally I was watching the film "Sixth Sense" last night - so can recommend the following (without adding spoilers). Some of which are already mentioned. So for fun:

     

    Temperature - not just a temperature guage but a sudden rate of change. It seemed to drop really quickly so you could get a value for that by differentiating an analog temperature sensor output and then using a comparator to trigger an alarm? You could also enter it in Back to Analog

     

    Very quiet audio - you'd need a way to ramp the gain up whilst negating any 'standard' room noise. Perhaps an Op-amp subtracting one microphone signal (directional in area of investigation) from the other (omni directional near user). You could also add a fast acting Automatic Gain Control (AGC) to limit loud sounds completely by blanking the audio out?

     

    The following are not in the film:

     

    Low Frequency Audio - seen that I'm sure in other films. A frequency multiplier circuit is needed.

     

    Audio Reverse Playback - when you get an audio recording it will most likely be backward (I've watched a few films so I know this is true, definately) so you'll need to reverse the recording to understand what they are saying.

     

    Conductivity of Air.  This might be fun (if not a bit dangerous), a high voltage unit to detect electrical breakdown of air.....all the paranormals create plasma etc.

     

    Air Pressure. Perhaps that changes before/during an event ?

     

    Mains Voltage. You need to enter Keithley Bench Digital Multimeter  as they will need to measure the mains voltage over a long duration. Again, in many films the light bulbs flicker or over-volt at the same time as an event.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 7 years ago

    Coincidentally I was watching the film "Sixth Sense" last night - so can recommend the following (without adding spoilers). Some of which are already mentioned. So for fun:

     

    Temperature - not just a temperature guage but a sudden rate of change. It seemed to drop really quickly so you could get a value for that by differentiating an analog temperature sensor output and then using a comparator to trigger an alarm? You could also enter it in Back to Analog

     

    Very quiet audio - you'd need a way to ramp the gain up whilst negating any 'standard' room noise. Perhaps an Op-amp subtracting one microphone signal (directional in area of investigation) from the other (omni directional near user). You could also add a fast acting Automatic Gain Control (AGC) to limit loud sounds completely by blanking the audio out?

     

    The following are not in the film:

     

    Low Frequency Audio - seen that I'm sure in other films. A frequency multiplier circuit is needed.

     

    Audio Reverse Playback - when you get an audio recording it will most likely be backward (I've watched a few films so I know this is true, definately) so you'll need to reverse the recording to understand what they are saying.

     

    Conductivity of Air.  This might be fun (if not a bit dangerous), a high voltage unit to detect electrical breakdown of air.....all the paranormals create plasma etc.

     

    Air Pressure. Perhaps that changes before/during an event ?

     

    Mains Voltage. You need to enter Keithley Bench Digital Multimeter  as they will need to measure the mains voltage over a long duration. Again, in many films the light bulbs flicker or over-volt at the same time as an event.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer