• Products and Partners
    Products and Partners
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
Member's Forum Building a 68000 single board computer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 632 subscribers
  • Views 2493 views
  • Users 0 members are here
  • Single Board Computer
  • 68000
  • home built
Related

Building a 68000 single board computer

2-zons
2-zons over 7 years ago

I have got an itch to build a 68000 bases computer.  It's been a long time since I've dabbled in this sort of thing.  In 1991 I build a 6809 based computer for school.  At the time I remember looking into the 68000 and how cool it was and seemed to be a wonder to program on, even compared to the wonderful 6809, and made X86 programming look like Egyptian hieroglyphs.  I am looking for a good schematic to base my computer off of.  Like I said it's been a while since I've done this sort of thing and I would like to start with a known working system and modify it from there.  Is this the right place to ask this sort of question?  If not is there a better place?

 

Thanks in advance, 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Unfortunately I don't have a schematic, but another option which has the fun of making a computer from a microprocessor, and similar instruction set, but using more modern parts and lower voltages, could be to use one of the other Freescale processors that were based on the 68k. For example the ColdFire range has processors to which you can attach RAM and Flash. It would be easier than the 68k in some ways, with the more modern parts (although even ColdFire is old, but still manufactured) - for example even the Palm handheld PDAs of the 1990's, which also had a 68k-compatible chip (the Freescale Dragonball) literally only needed two additional chips, the SRAM and Flash, and zero glue logic. I had fun building a Palm-type device using that chip.

    ColdFire has hand-solderable options (QFP package).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Unfortunately I don't have a schematic, but another option which has the fun of making a computer from a microprocessor, and similar instruction set, but using more modern parts and lower voltages, could be to use one of the other Freescale processors that were based on the 68k. For example the ColdFire range has processors to which you can attach RAM and Flash. It would be easier than the 68k in some ways, with the more modern parts (although even ColdFire is old, but still manufactured) - for example even the Palm handheld PDAs of the 1990's, which also had a 68k-compatible chip (the Freescale Dragonball) literally only needed two additional chips, the SRAM and Flash, and zero glue logic. I had fun building a Palm-type device using that chip.

    ColdFire has hand-solderable options (QFP package).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • 2-zons
    0 2-zons over 7 years ago in reply to shabaz

    That sounds very interesting.   I have heard of this chip while doing research for my build.  It sounds interesting.  What would be the equivalent of an EPROM in that type of system?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer