Member's Forum Flashing Led's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 53 replies
  • Answers 23 answers
  • Subscribers 634 subscribers
  • Views 6673 views
  • Users 0 members are here
  • blink led
Related

Flashing Led's

commanderkelly
commanderkelly over 7 years ago

Hello, I am new to this site and loving it. I did a bit of Electronics in 1995 where I made a flashing led circuit with 2 led's and it was cool. My other hobby is model trains and I would like to put 2 small led's in buffer stops and make them flash and run it off a DC train controller. Does anyone have a simple circuit that would do the job for this? I am basically a noob at electronics but I can follow a simple circuit.

 

Thank you.

 

Gary.

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    0 14rhb over 7 years ago

    To everyone following commanderkelly initial blog, I must admit there are some strange goings on for such a simple circuit image

     

    Like fmilburn I also breadboarded this to see how supply voltage affected the flash rate. I used 2N3804 transistors, 68k + 10uF/25v capacitors, plain old technology LEDs + 560 ohm current limiting resistors. These component values give a decent 1.22 Hz flash rate at 14v DC.

     

    The flash rate did vary, and it increased as the voltage dropped to around that required by the LEDs...as expected. Mid-voltages I saw a flash rate as expected, as seen in the blue plot below. This was based on the following equation:

    frequency      = 1 / (0.38 * R * C)

                          = 1.06Hz image

    But at higher voltages the flash rate started to increase again and I wasn't sure why. I don't think it is to do with the capacitors: for some types of capacitor the capacitance value changes significantly with applied voltage, but that isn't the case for electrolytics. I ran the circuit without the LEDs and measured the frequency on an oscilloscope and it still exhibited this variance in frequency. That leaves the effect down to the transistors.

     

    Focusing on the voltages on the transistor, and specifically the base voltage (which goes negative during switching and the capacitor voltage is maintained but inverts) this reverse biased the base-emitter junction of the transistor....there is a rated value in the specification sheets for that of 6v minimum. I suspect when that is overcome the junction behaves like a Zener diode, something we did not expect. Now the timing will start to vary as we see in the blue plots above. There is a solution though. Adding a simple diode like the 1N4148 in series with the base of both transistors prevents this effect occuring as these diodes now increase that breakdown voltage significantly to approx. 75v.

     

    Plotting the frequency now gives the orange graph above. We can see the circuit behaves poorly at low voltages as it now has to overcome the forward bias of the new diode to start working. But at higher voltages it definately looks much better.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 7 years ago in reply to 14rhb

    Great detective work Rod!  Good on you for for actually measuring frequency at higher voltage as I missed that. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 7 years ago in reply to 14rhb

    Great detective work Rod!  Good on you for for actually measuring frequency at higher voltage as I missed that.