• Products and Partners
    Products and Partners
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
Member's Forum Flashing Led's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 53 replies
  • Answers 23 answers
  • Subscribers 634 subscribers
  • Views 6952 views
  • Users 0 members are here
  • blink led
Related

Flashing Led's

commanderkelly
commanderkelly over 7 years ago

Hello, I am new to this site and loving it. I did a bit of Electronics in 1995 where I made a flashing led circuit with 2 led's and it was cool. My other hobby is model trains and I would like to put 2 small led's in buffer stops and make them flash and run it off a DC train controller. Does anyone have a simple circuit that would do the job for this? I am basically a noob at electronics but I can follow a simple circuit.

 

Thank you.

 

Gary.

  • Sign in to reply
  • Cancel
Parents
  • SGarciaV
    0 SGarciaV over 7 years ago

    Hi Gary. I see that you've gotten lots of great responses. Personally, I am partial to the 555 :-D

     

    I recently built a circuit similar to the one described in the following video:

     

    https://youtu.be/gYnd_nMi39g

     

    As for the Arduino, once you have the board you need to install the Arduino IDE. You can get that at the following link:

     

    https://www.arduino.cc/en/main/software

     

    Two important settings of the IDE that *must* be correct are the serial port designation and the board type. There are lots of Arduino models, such as Uno, Nano, Mega, Leonardo and many more from other vendors. To get started, I would purchase one that is compatible with either the Uno or Nano.

     

    If the Arduino IDE is open, close it. Connect the Arduino to the PC via the provided USB cable. Note that the Uno uses a different cable than the Nano (for example).

     

    Once the Arduino is connected to the PC, the OS should recognize it and assign a serial port to it. Note that my experience and comments are in regard to a Windows installation.

     

    Now launch the Arduino IDE. Locate the settings for the port and select the port that was assigned to the Arduino that you connected. Also select the correct board.

     

    Go to the File menu option and open the Blink example. This is a really simple program, which in the Arduino world programs are called sketches, that blinks the internal LED. Once the program is open, click on the button to compile and download the sketch to the Arduino. If you get an error, check that the Arduino is connected and also check that you selected the correct serial port and board.

     

    Search E14 and Youtube, there are lots of tutorials to get you started. Here is one possible video:

     

    https://youtu.be/kLd_JyvKV4Y

     

    Sorry, at 37 minutes, I don't have time to watch it to comment on the video. Also search for Jeremy Blum's Arduino videos. Hopefully this info will be helpful to you. Good luck on your projects and welcome to Element 14, where everyone knows Ohm's Law! ;-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 6 years ago in reply to SGarciaV

    I too have a fond liking for the 555 having used it for many projects through the 80's/90's. It was amazing what projects that IC could be used for and indeed people wrote whole books on the subject.

     

    However I will often now undertake such projects using a PIC microcontroller that operates on its own internal clock. Some of these 8-bit MCU have very small footprints. The timing is extremely accurate (for LED flashing anyway), they can be reconfigured easily and have almost no other components. I used a very small Surface Mount Technology device (SMT) on this quick project ledog - Light Emitting Dog

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • parachaser
    0 parachaser over 6 years ago in reply to 14rhb

    The 555 timer is an IC chip that every Electronics enthusiast should have an abundance of and the PN2222A transister. Just sayin !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • parachaser
    0 parachaser over 6 years ago in reply to 14rhb

    The 555 timer is an IC chip that every Electronics enthusiast should have an abundance of and the PN2222A transister. Just sayin !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • commanderkelly
    0 commanderkelly over 6 years ago in reply to parachaser

    I got some of them a few months back, but not really done much of anything on Electronics. I am hoping to start back up again now.