• Products and Partners
    Products and Partners
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
Member's Forum Flashing Led's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 53 replies
  • Answers 23 answers
  • Subscribers 634 subscribers
  • Views 6971 views
  • Users 0 members are here
  • blink led
Related

Flashing Led's

commanderkelly
commanderkelly over 7 years ago

Hello, I am new to this site and loving it. I did a bit of Electronics in 1995 where I made a flashing led circuit with 2 led's and it was cool. My other hobby is model trains and I would like to put 2 small led's in buffer stops and make them flash and run it off a DC train controller. Does anyone have a simple circuit that would do the job for this? I am basically a noob at electronics but I can follow a simple circuit.

 

Thank you.

 

Gary.

  • Sign in to reply
  • Cancel
Parents
  • commanderkelly
    0 commanderkelly over 7 years ago

    I have not been well for a bit but have not forgot about this project. I have now got one of them Ardunio Uno and was thinking of powering the flashing leds with it in the buffer stops. Now as I said before I am a noob at all this and I have no clue how to use an Arduino, Can anyone help me out here. I would like to power say like 10 flashing leds on differant buffer stops around the train track. Would this be possible on 1 Arduino and does anyone have a circuit that would help me do this.

     

    Thank you Gary.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to commanderkelly

    Hi Gary,

     

    It can do that, there's an example for a single LED here:

    https://www.arduino.cc/en/tutorial/blink

     

    Once you've tried that, then you'll have confirmed the software and hardware is functioning, and then you can extend it to more LEDs to achieve your aim. Extending to flash two LEDs alternatively is easy by slightly modifying this code.

    However, it wasn't clear what behaviour you were looking for. If it is to flash all LEDs identically or flash all LEDs in alternate pairs, then the code doesn't need to change further, you can connect many LEDs to the same connections on the Arduino, although you'll need to use some small additional circuit to provide the current for all the LEDs. Is this what you're aiming to do?

    Otherwise, if your aim is to make them flash at different rates, or alternately, or under control of individual switches or sensors, then that will need more code changes.

    The easiest way is to start with the blink example mentioned, and then try a few more examples, to get familiar with the capabilities of the Arduino. Then you'll feel confident to want to do more complex behaviour for the LEDs (e.g. controlled by switches as mentioned).

     

    The tutorials here: https://www.arduino.cc/en/Tutorial/BuiltInExamples   will give you a feel for the capabilities of the Arduino (not all need to be tried, just a few that interest you).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • commanderkelly
    0 commanderkelly over 7 years ago in reply to shabaz

    Hello and thank you I just want them to flash at the smae rate so for now this will do, thanks for your help.

     

    Gary

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • commanderkelly
    0 commanderkelly over 7 years ago in reply to fmilburn

    The Arduino UNO did it for me, just what I want. 1. tryed with 1 Led flashing2. added another led where both was flassing at same time. I want to Thank everyone who as helped me with this project really nice people, I am sure I will play with this to make them flash at different times.imageimage

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 7 years ago in reply to commanderkelly

    PS:  it should be much easier with an Arduino than all the mucking about we did above :-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 7 years ago in reply to commanderkelly

    Hi Gary,

     

    If you are OK with them flashing at the same rate and more or less synchronized then it is fairly straightforward  with an Arduino and will work just as Shabaz has described.  The circuit will be simple. There can be 10 output pins connected to the LEDs with current controlling resistors of say 330 ohms.  There could be 10 input pins for switching the behavior of the LEDs.  When a switch signals the start a timer can be used to determine how long the blinking occurs.  It is an interesting project.  Once you get things working as Shabaz describes then report back if it is not clear on how to proceed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 7 years ago in reply to commanderkelly

    Hi Gary,

     

    If you are OK with them flashing at the same rate and more or less synchronized then it is fairly straightforward  with an Arduino and will work just as Shabaz has described.  The circuit will be simple. There can be 10 output pins connected to the LEDs with current controlling resistors of say 330 ohms.  There could be 10 input pins for switching the behavior of the LEDs.  When a switch signals the start a timer can be used to determine how long the blinking occurs.  It is an interesting project.  Once you get things working as Shabaz describes then report back if it is not clear on how to proceed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer