• Products and Partners
    Products and Partners
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
Member's Forum MIFH1 Connector Identification
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 631 subscribers
  • Views 969 views
  • Users 0 members are here
  • component identification
  • board connector
  • identify
Related

MIFH1 Connector Identification

techrocket9
techrocket9 over 6 years ago

I have a Mitsubishi heat pump which was installed with the worst wireless thermostat I've ever used -- a MRCH1.

 

Fortunately, it turns out that the pump is controlled via UART. The wire protocol has already been reversed, but to do this cleanly I want to put my replacement controller (A Pi 0 W) where the existing wireless control board is, and use the existing cable run to that location.

 

This is the cable in question (another link). I know that the red connector on the heat pump end is a CN105, but I don't know what the black connector is on the other end. This black connector is what I have access to in the location I want to install the new controller.

 

I'm making this post in hopes that someone here has seen the black connector before and can identify it. I need to purchase/make a female connector for it so I can wire it up to my Pi.

 

I've uploaded an album with pictures of the connector (both the male and female ends) here.

Any help you can provide to identify the connector is appreciated.

Cheers,

 

-- Techrocket9

Edit: My calipers measure the distance between the center of the pins as 2.55mm. The external width of the female connector is 16.32mm, and the depth (not counting the wire coming out the back of it) is 13.53mm. The external width of the male connector is 12.66mm,  and its minimum external height is 2.54mm.


  • Sign in to reply
  • Cancel
Parents
  • techrocket9
    0 techrocket9 over 6 years ago

    It actually ended up being this particular molex connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • techrocket9
    0 techrocket9 over 6 years ago

    It actually ended up being this particular molex connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer