• Products and Partners
    Products and Partners
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
Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 7151 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    I've used lots of Traco DC-DC converters and found them to be reliable but quite noisy (no worse than other makes at similar prices) so output filtering may be helpful.

    The other issue is that the start up current of the Traco converters can be quite high, so while you may have a run current of 150mA you might need 700mA to get it to start - worth testing in a lashup if you can.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to michaelkellett

    This discussion has pushed me to do something I was planning since some time: make a power supply for my eload.

    I'm a known procrastinator. I need a push to do somethng that's not on my immediate horizon. This thread made that happen image.

    I'm turning the evaluation board of the Infineon Gate Driver with Truly Differential Input - Review into the supply for the analog part.

     

    image

     

    michaelkellett  wrote:

     

     

    The other issue is that the start up current of the Traco converters can be quite high, so while you may have a run current of 150mA you might need 700mA to get it to start - worth testing in a lashup if you can.

     

    MK

     

    I will test that, Michael, and share the results here ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Jan Cumps

    I'll look forward to see the results !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    The Traco behaves OK, powered from a Meanwell 48 V, 1.25 A brick. (48 V is the nominal input power for the Traco TEN 6-4xxTraco TEN 6-4xx series I'm using here).

     

    Because it powers the analog side, I'll include a filter circuit. The analog side would then be powered from the filter output. I'd power the fan directly from the Traco output, before the filter ...

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Jan Cumps

    Hello Jan,

    I've never investigated in detail - just observed the current limit setting needed on the bench PSU to get them up and running.

     

    I think I still have boards with TRACOs on somewhere - I'll try lighting one up later this weekend.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    1.4 A is because I put my meter in the 1 A range. 1.4 is the limit then. If I put it in the 10 A range, it also peaks out.

    That's normal. The input capacitor is a shortcut initially. Only the PSU impedance, the test leads and the capacitor's ESR restrict the inrush.

    it's only a few samples wide. There's virtually no energy there. Every hard-switched DC circuit with an input capacitor has this phenomena.

    The capacitor in my circuit is 47uF.

     

    Input capacitors cause inrush. The more capacitance, the higher the inrush energy. 220 uF would increase the (not really a) drama...

     

    edit: you don't have to worry about it. You just need to take care that you have enough oooomph in the supply to get going and deliver the nominal current once stable. It would only be an issue if your source collapses under the initial demand and doesn't recover.

     

     

    Here's what the output switch-on curve  looks like, with 125 mA current (96 Ohm load):

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I mentioned the inrush, as the data sheet mentions it in respect to inrush voltage.  It suggests using a 220uF 100V electrolytic in front of the component to manage this - from your photo, it would look like there is a large electrolytic but I couldn't see what it was.  1.4A is a lot though - I'll have to watch out for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I mentioned the inrush, as the data sheet mentions it in respect to inrush voltage.  It suggests using a 220uF 100V electrolytic in front of the component to manage this - from your photo, it would look like there is a large electrolytic but I couldn't see what it was.  1.4A is a lot though - I'll have to watch out for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    The Traco behaves OK, powered from a Meanwell 48 V, 1.25 A brick. (48 V is the nominal input power for the Traco TEN 6-4xxTraco TEN 6-4xx series I'm using here).

     

    Because it powers the analog side, I'll include a filter circuit. The analog side would then be powered from the filter output. I'd power the fan directly from the Traco output, before the filter ...

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    1.4 A is because I put my meter in the 1 A range. 1.4 is the limit then. If I put it in the 10 A range, it also peaks out.

    That's normal. The input capacitor is a shortcut initially. Only the PSU impedance, the test leads and the capacitor's ESR restrict the inrush.

    it's only a few samples wide. There's virtually no energy there. Every hard-switched DC circuit with an input capacitor has this phenomena.

    The capacitor in my circuit is 47uF.

     

    Input capacitors cause inrush. The more capacitance, the higher the inrush energy. 220 uF would increase the (not really a) drama...

     

    edit: you don't have to worry about it. You just need to take care that you have enough oooomph in the supply to get going and deliver the nominal current once stable. It would only be an issue if your source collapses under the initial demand and doesn't recover.

     

     

    Here's what the output switch-on curve  looks like, with 125 mA current (96 Ohm load):

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer