• Products and Partners
    Products and Partners
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
Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 7158 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
Parents
  • Andrew J
    0 Andrew J over 6 years ago

    The isolator arrived and I hooked it up - in the end I went for a Recom RS6-1205S.  It's very similar to the Traco one, a bit cheaper.  It actually works for what I want to do: using it to power Side A of the i2c and digital isolators as well as the Arduino.  I did some quick measurements:

     

    Initially load was just a 1K resistor:

    AC with 0.1uf and 1uf capacitor on the output:

    image

    DC with 0.1uf and 1uf capacitor on the output:

    image

    AC with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

    image

    DC with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

    image

    Powering side A, still with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

     

    AC:

    image

    DC:

    image

     

    It's quite noisy, as Michael alluded to, and there is quite a large amount of ripple induced on the DC (datasheet states 25mV to 75mV) but it's on a breadboard without any great output filtering.  I still need to work through any impact this has on Side b (where the DAC and ADC are located.)  In theory, I would expect none as they are driven through I2C commands and the DAC is powered from a REF5040 which is used as the reference source for the DAC output.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago

    The isolator arrived and I hooked it up - in the end I went for a Recom RS6-1205S.  It's very similar to the Traco one, a bit cheaper.  It actually works for what I want to do: using it to power Side A of the i2c and digital isolators as well as the Arduino.  I did some quick measurements:

     

    Initially load was just a 1K resistor:

    AC with 0.1uf and 1uf capacitor on the output:

    image

    DC with 0.1uf and 1uf capacitor on the output:

    image

    AC with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

    image

    DC with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

    image

    Powering side A, still with 0.1uf, 1uf and 10uf (electrolytic) capacitor on the output:

     

    AC:

    image

    DC:

    image

     

    It's quite noisy, as Michael alluded to, and there is quite a large amount of ripple induced on the DC (datasheet states 25mV to 75mV) but it's on a breadboard without any great output filtering.  I still need to work through any impact this has on Side b (where the DAC and ADC are located.)  In theory, I would expect none as they are driven through I2C commands and the DAC is powered from a REF5040 which is used as the reference source for the DAC output.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer