• Products and Partners
    Products and Partners
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
Member's Forum Those insulated strands
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 631 subscribers
  • Views 631 views
  • Users 0 members are here
Related

Those insulated strands

steveweber
steveweber over 6 years ago

So my son broke his wired headphones recently. The strands of the left and right channel wires seem to insulated. I've read a blog and saw a video in which the recommended approach is to apply a momentary flame to get to bare strands. Is this for real? Hope someone has a better suggestion. Thanks.

  • Sign in to reply
  • Cancel
  • steveweber
    0 steveweber over 6 years ago

    Thank you for these quick and inciteful responses. Will try the solder bubble method. Now that I have some good options I'm ready to tackle this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago

    I had an Ungar soldering iron with a clip on the heater barrel that looked like a section of dull knife blade with a V notch in it.

    It was used to strip delicate wires without damaging the wire by melting the insulation as it was scraped off the wire. It worked on insulation that would melt. It didn't work well on Teflon or enamel insulation.

    You can buy better thermal wire strippers, but not likely worth buying for one repair job.

    If you heat up a small screw driver blade it might work.

    It is tough to make a small splice joint look good. If you are doing multiple wires at the joint, it is worth staggering them at different lengths so they have less chance of shorting to each other and the joint can be much slimmer. A small piece of heat shrink tube over the joint is about as clean as you will get.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 6 years ago

    The suggestion is one method to break down the insulation to expose the conductor. If you elect to use the procedure make sure you do it in a well ventilated areas. Fumes from burning some conductor insulation can be toxic.

     

    The wire inside a transformer looks bare but is insulated with a lacquer. Heating the coating causes it to melt exposing the conductor. You can also scrape the insulation off using a very sharp knife.

     

    Wire can be thinner if the insulation is reduced. By the sound of your description, the wire is very small and the insulation is minimal. I have never used direct flame (i.e. lighter) to remove the insulation L-G suggestion of a soldering iron should work.

     

    Have you found a break in the conductor that needs to be repaired. What about replacing the whole conductor end to end eliminating the need to splice. The ends of the conductor are no doubt solder exposed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago

    You could do that or the heat from the soldering iron can be sufficient, especially if you try to tin it in a bubble of solder. Much of the thinner wires and coating are considered "self fluxing enamel" and thus can just be "soldered through". Thicker enamel may require scraping by blade.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer