Member's Forum What is the best electronics deal you ever scored?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 635 subscribers
  • Views 3182 views
  • Users 0 members are here
  • fleamarkets
  • electronics deals
Related

What is the best electronics deal you ever scored?

dougw
dougw over 5 years ago

I am sure I have scored some great deals over the years and probably the road tests and contest winnings I've had on element14 would rank as the best deals I ever had.

I am asking this question because I am sure the answers will trigger some great memories of deals I found along the way.

I do remember one one auction I went to where I got a box of fifteen brand new 9V transformers for about $20. These things were perfect for 5 to 12 V linear power supplies. They were big - about 15 amp outputs and they were so heavy I had to sell half of them to the guys I was bidding against, just so I could carry the rest in my back-pack. But it also meant I got all I could carry almost for free.

Those flea markets and Ham fests and electronics auctions seem to have disappeared from this area.

If you have a picture of your great deal, all the better...

  • Sign in to reply
  • Cancel
Parents
  • ajcc
    0 ajcc over 5 years ago

    My KENWOOD PW18-2 linear power supply that I got for €30 plus shipping from an online auction site. It was listed under home/consumer electronics, not in the test gear section, so no one else saw it. It's a split-rail +/- 18 Volt supply with a 2 Amp max rating, so it's not the most powerful supply and digital boards are often too much for it.

     

    But it has served me really well during the 5½ years I've had it, and has enabled me to work on labs after hours while taking EE classes. At home you can even bring warm tea into the lab, so that alone is worth the €30 image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ajcc
    0 ajcc over 5 years ago

    My KENWOOD PW18-2 linear power supply that I got for €30 plus shipping from an online auction site. It was listed under home/consumer electronics, not in the test gear section, so no one else saw it. It's a split-rail +/- 18 Volt supply with a 2 Amp max rating, so it's not the most powerful supply and digital boards are often too much for it.

     

    But it has served me really well during the 5½ years I've had it, and has enabled me to work on labs after hours while taking EE classes. At home you can even bring warm tea into the lab, so that alone is worth the €30 image

    • Cancel
    • Vote Up +7 Vote Down