Member's Forum What is the best electronics deal you ever scored?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 635 subscribers
  • Views 3169 views
  • Users 0 members are here
  • fleamarkets
  • electronics deals
Related

What is the best electronics deal you ever scored?

dougw
dougw over 5 years ago

I am sure I have scored some great deals over the years and probably the road tests and contest winnings I've had on element14 would rank as the best deals I ever had.

I am asking this question because I am sure the answers will trigger some great memories of deals I found along the way.

I do remember one one auction I went to where I got a box of fifteen brand new 9V transformers for about $20. These things were perfect for 5 to 12 V linear power supplies. They were big - about 15 amp outputs and they were so heavy I had to sell half of them to the guys I was bidding against, just so I could carry the rest in my back-pack. But it also meant I got all I could carry almost for free.

Those flea markets and Ham fests and electronics auctions seem to have disappeared from this area.

If you have a picture of your great deal, all the better...

  • Sign in to reply
  • Cancel
  • the-dubster
    0 the-dubster over 5 years ago

    I got a lovely Denon amplifier about 20 years ago for a roll of 2.5mm Twin and Earth - which I 'acquired' from stores (if it has a NATO Stock Number . . . . . . ) and then used the Station Supply and Movements Section to send to the other base.

     

    Got the amplifier by return a few days later . . .

     

     

    Free basically, and it still works great to this day.

     

     

     

    Oh, and a few years working at Sealand and being the IC of a Test Measurement Equipment Cell did get me a couple of old CRT Scopes and a nice Ver 1.0 Fluke 89 -  the less said about those the better . . . . .

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago

    A Thorens TD-124 at a garage sale for 12€.

     

    image

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajcc
    0 ajcc over 5 years ago in reply to Fred27

    Fred27 They used to have a 4/30 (MSP430 day) deal, but I don't think they've had that in 2019 or 2020? I bought a MSP-EXP430FR2433 LaunchPad in 2018 and a MSP430G2553IN20MSP430G2553IN20 to upgrade my old MSP-EXP430G2 LaunchPad. Really should do more projects with them, the built in debugger is such a nice feature of those boards.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 5 years ago

    Mostly the winnings from Element 14.

     

    I did bid for a ‘working perfectly’ Fluke 287 on the flea, and got that for a bargain.  Apart from a blown power cap and damaged battery terminals it was ‘perfect’ as long as you didn’t need to use it for more than a few days and had a massive stash of AA batteries.  Toe rag!!  However, it turns out those things have a lifetime warranty and whilst I could have fixed it myself - the cap is a well known problem - I thought I’d send it to Fluke.  In less than a week, they’d sent me a brand new one to replace it!  I call that a great result and excellent customer service.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Fred27
    0 Fred27 over 5 years ago

    I agree that some of the best "scores" are the road tests here on E14, but excluding those:

     

    A MSP430 development kit for $4.30. That used to be the official list price (including international shipping) so I didn't get a deal in that sense. However that was my ridiculously low price of entry into the world of embedded development. A gateway drug.

    A Proliant DL380G5 rack mount server from eBay - £18. The "local collection only" meant a fairly substantial server cost me less than a Raspberry Pi.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajcc
    0 ajcc over 5 years ago

    My KENWOOD PW18-2 linear power supply that I got for €30 plus shipping from an online auction site. It was listed under home/consumer electronics, not in the test gear section, so no one else saw it. It's a split-rail +/- 18 Volt supply with a 2 Amp max rating, so it's not the most powerful supply and digital boards are often too much for it.

     

    But it has served me really well during the 5½ years I've had it, and has enabled me to work on labs after hours while taking EE classes. At home you can even bring warm tea into the lab, so that alone is worth the €30 image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 5 years ago

    Hi Doug!

     

    The best deal that comes to mind for me is the 130-in-1 kit I bought about 15 years ago at a deep discount from Radio Shack (or was it The Source already?). Partly because it was a good deal in itself, but mainly because it kick-started me back into my tech hobby image

    I've since given it away to help kickstart someone else's passion for tech.

     

    -Nico

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
<