• Products and Partners
    Products and Partners
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
Member's Forum Suggestions for C Language IDE?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 12 answers
  • Subscribers 635 subscribers
  • Views 3443 views
  • Users 0 members are here
  • c language
  • visual studio 2019
  • eclipse ide
  • c-c++ programming
  • c code
  • c programing language
Related

Suggestions for C Language IDE?

mudz
mudz over 5 years ago

Which IDE you use or have used for C programming? Which one you like the most and why?

/﹋\

(҂`_´)

<,︻╦╤─ ҉      c c c c c c c c c c c c c   ▬▬▬.◙.▬▬▬

  /﹋\                                                     ═▂▄▄▓▄▄▂

                                                            ◢◤ █▀▀████▄▄▄▄◢◤

                                                            █▄ █ █▄ ███▀▀▀▀▀▀▀╬

                                                            ◥█████◤

                                                            ══╩══╩═

 

Update ------

Spent a lot of time on eclipse but wasn't able to get it in working mode, Tried Visual studio again and it worked just needed a little bit of tinkering. it worked but output .exe false detected by Bitdefender antivirus and got quarantined automatically. Added folder to exceptions. Hmmm, may be VS not that bad ! Lets c how it goes.
Will definitely keep working on eclipse, will learn things doing so.

I'll keep on updating !!
Thank you all 
image

 

p.s- This discussion isn't over yet, all suggestions are most welcome.

 

Message was edited by: mudz

 

Update 2 ------

Interestingly I did something, and it worked. So, eclipse is working as well for now. I've no idea. Cygwin64 to mingw.. ¯\_(ツ)_/¯

 

Message was edited by: mudz

  • Sign in to reply
  • Cancel
Parents
  • jomoenginer
    0 jomoenginer over 5 years ago

    What OS are you working with?

     

    On Linux, for just simple C development, either vi or vim.  With vim you can add features where you can do syntax highlighting and such.

    For IDE specific, Eclipse would be the first one.

    Code::Blocks is another one which is cross platform: Windows, Linux, Mac OS X, Raspberry Pi.

    Visual Studio Code as an Editor with compile done via command line but working on using it as a compiler.

    Atom is another simple editor.

     

    Windows: Eclipse, Visual Studio, Visual Studio Code pretty much in that order.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jomoenginer
    0 jomoenginer over 5 years ago

    What OS are you working with?

     

    On Linux, for just simple C development, either vi or vim.  With vim you can add features where you can do syntax highlighting and such.

    For IDE specific, Eclipse would be the first one.

    Code::Blocks is another one which is cross platform: Windows, Linux, Mac OS X, Raspberry Pi.

    Visual Studio Code as an Editor with compile done via command line but working on using it as a compiler.

    Atom is another simple editor.

     

    Windows: Eclipse, Visual Studio, Visual Studio Code pretty much in that order.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer