• Products and Partners
    Products and Partners
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
Member's Forum Finding the logic in remote control data
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 630 subscribers
  • Views 1686 views
  • Users 0 members are here
  • 433.92mhz
  • remote controlled
  • radio receiver
Related

Finding the logic in remote control data

obones
obones over 5 years ago

I have a set of remote controlled power sockets which operate on the 433MHz range and am trying to understand the protocol used between the remote and the sockets. They are sold under the Silvercrest brand, with the 284705 IAN.

 

Using an ESP32 with a RFM69CW module, I was able to figure out that it uses OOK PWM transmission to send packets of 24 bits for each order, and that the first 4 are the remote Id, the last 4 are the button Id.

 

This leaves me with the 16 middle bits for which I observed they can only take 4 possible values for a given button and order. For instance, pressing the "On" order for button "A" sends one of the following four values, in a repeating loop:

 

    F756

    7441

    D9C5

    E3AA

 

I thought that this might be a rolling code, but using again the ESP32 to send commands, I discovered that the socket reacts to any one of the following 4 codes. I can even send always the same, it will react properly and this has no impact on the remote usage.

 

Giving the "Off" order for button "A" uses a different set of four values:

 

    20E7

    5212

    9D88

    8C0B

 

Button B uses a different set of values, for On:

 

    6AF3

    453F

    0F6E

    C170

 

and for Off:

 

    16BC

    3B99

    B8DD

    AE24

 

On the same remote, there are three other buttons, C, D and Master, but C and Master use the same set of codes as A while D uses the same codes as B, just with a reversed meaning. This is easily figured out by looking at bit 1 of the button 1. If it's a 1, then the meaning is reversed.

 

I could easily use a lookup table for those values and be done with it, but I have found other people using those remote controlled sockets and it appears they are receiving other codes for the "On"/"Off" command. One such example is here.

 

So, what I'd like to figure out is the relationship between a given set of four codes, basically a "formula" that allows to validate any code, based on one of the three others and figure out if it's "On" or "Off" in the process, pretty much like what the socket is doing when it receives a command.

 

I tried counting bits, XORing, ANDing, ORing each pair of values, but nothing seemed obvious to me.

 

Does this appear easy to any of you?

What would you suggest I try next?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    obones  wrote:

     

     

    What would you suggest I try next?

    Suggest determining if it's worth your time trying to figure it out : ) What problem would it solve? You only need to store a few bytes more in Flash if you wish to send all the four codes in the cycle to replicate the transmitter behavior 100%.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago

    obones  wrote:

     

     

    What would you suggest I try next?

    Suggest determining if it's worth your time trying to figure it out : ) What problem would it solve? You only need to store a few bytes more in Flash if you wish to send all the four codes in the cycle to replicate the transmitter behavior 100%.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • obones
    0 obones over 5 years ago in reply to shabaz

    Well, that's already what I do, I have a truth table for my own remote and it works.
    But I have two issues with the current situation

     

    1. I would like to create a "universal" code and there are other remotes for the same kind of plugs that appear to use other codes, as shown in the linked github project.
    2. I don't like hard coded truth table, my brain always itches when I could not figure out the entire logic

     

    So, yes, I could leave it as is, but the itching in my brain will stay there ;-)