• Products and Partners
    Products and Partners
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
Member's Forum Finding the logic in remote control data
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 630 subscribers
  • Views 1684 views
  • Users 0 members are here
  • 433.92mhz
  • remote controlled
  • radio receiver
Related

Finding the logic in remote control data

obones
obones over 5 years ago

I have a set of remote controlled power sockets which operate on the 433MHz range and am trying to understand the protocol used between the remote and the sockets. They are sold under the Silvercrest brand, with the 284705 IAN.

 

Using an ESP32 with a RFM69CW module, I was able to figure out that it uses OOK PWM transmission to send packets of 24 bits for each order, and that the first 4 are the remote Id, the last 4 are the button Id.

 

This leaves me with the 16 middle bits for which I observed they can only take 4 possible values for a given button and order. For instance, pressing the "On" order for button "A" sends one of the following four values, in a repeating loop:

 

    F756

    7441

    D9C5

    E3AA

 

I thought that this might be a rolling code, but using again the ESP32 to send commands, I discovered that the socket reacts to any one of the following 4 codes. I can even send always the same, it will react properly and this has no impact on the remote usage.

 

Giving the "Off" order for button "A" uses a different set of four values:

 

    20E7

    5212

    9D88

    8C0B

 

Button B uses a different set of values, for On:

 

    6AF3

    453F

    0F6E

    C170

 

and for Off:

 

    16BC

    3B99

    B8DD

    AE24

 

On the same remote, there are three other buttons, C, D and Master, but C and Master use the same set of codes as A while D uses the same codes as B, just with a reversed meaning. This is easily figured out by looking at bit 1 of the button 1. If it's a 1, then the meaning is reversed.

 

I could easily use a lookup table for those values and be done with it, but I have found other people using those remote controlled sockets and it appears they are receiving other codes for the "On"/"Off" command. One such example is here.

 

So, what I'd like to figure out is the relationship between a given set of four codes, basically a "formula" that allows to validate any code, based on one of the three others and figure out if it's "On" or "Off" in the process, pretty much like what the socket is doing when it receives a command.

 

I tried counting bits, XORing, ANDing, ORing each pair of values, but nothing seemed obvious to me.

 

Does this appear easy to any of you?

What would you suggest I try next?

  • Sign in to reply
  • Cancel
Parents
  • javagoza
    0 javagoza over 5 years ago

    I think the same as shabaz

    but if it is just for curiosity, have you tried to decode the data as a Manchester code? Manchester code - Wikipedia

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • javagoza
    0 javagoza over 5 years ago

    I think the same as shabaz

    but if it is just for curiosity, have you tried to decode the data as a Manchester code? Manchester code - Wikipedia

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • obones
    0 obones over 5 years ago in reply to javagoza

    The RF signal that I receive is OOK PWM, meaning that I have a series of Long/Short and Short/Long "High/Low" pairs. This is what I decoded to get the 24 bits and establish the truth table presented above.
    What you are suggesting is that I take those mystery 16 bits and apply Manchester decoding onto them?
    So for instance, I have e3aa which in binary is 1110001110101010 and I should interpret this as a series of raising and falling edges?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer