• Products and Partners
    Products and Partners
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
Member's Forum Steel Conduit - How to Install ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 10 answers
  • Subscribers 633 subscribers
  • Views 6576 views
  • Users 0 members are here
  • galvanised_conduit
  • 25mm conduit
  • conduit_installation
  • electrical
  • conduit
Related

Steel Conduit - How to Install ?

14rhb
14rhb over 5 years ago

Looking around the internet I've found very little to help me understand how electrical steel conduit is installed.....but I'm sure someone on Element14 knows the answers image

 

The question relates to the 20/25mm galvanised steel conduit often used in the UK - this comes as 3m lengths with a external make thread on one end and a female coupler on the other. Unless the fittings are 3m apart the conduit requires cutting and a new thread to be formed, which I already have tools for. The outlets/fixings also come with pre-cut threads; and example of the 90 degree box is shown below:

image

Whilst I can envisage fixing one of the box outlets to the required position and screwing in a piece of cut/pre-threaded conduit I wonder how the next fitting is added. Assuming that is a cut end which I have added a thread to this second fixing would need rotating onto the conduit. Because the first fixing is on the wall there would be no clearance to rotate the second fixing without putting strain on the existing system, this is especially true when the next fitting has additional bosses on it or as the system design grows.

 

Maybe the entire system is designed and then mounted to the wall ? I would imagine that could result in a very heavy setup plus inaccuracies in getting the fittings where required.

 

Any pointers would be gratefully read, thank you image

  • Sign in to reply
  • Cancel
Parents
  • chunkasmaximus
    0 chunkasmaximus over 5 years ago

    As with everything in life Rod H, practice makes perfect!

     

    Donald Lane's answer pretty much sums it up.

     

    You just have to work methodically and in one direction - don't try starting at two different points and meeting in the middle!

     

    I've not looked at what advice or videos are available, but as an electrician who has used the stuff on and off since college, the best advice I can sum up is the following (in no particular order):

     

    1. Practice and experiment joining different sections of conduit, boxes, accessories etc in small sections (using off cuts etc), then dismantle and reassemble. This will enable you to get used to doing things in the most efficient order. There's nothing worse than getting to a point, only to realise you have to undo it all. This will also help you with the planning of slightly larger scale installs, so you'll be less reliant on others for help.

     

    2. Use all the available fittings for your conduit system to make your life easier. Like already suggested in other comments, use fittings like running couplers, nipples, lock rings, bushes and the like. This will give you more flexibility and make assembly a little easier.

     

    3. Make the conduit bender your best buddy. A floor standing one is ideal, with a built-in vice if you can. It will be painful and it will take time but, the more you use it the less joints you'll have, the easier it will be to pull cables, and the neater it will look. It really is an art form, and if you plan to work with steel conduit long term, this is definitely a worthwhile investment.

     

    4. Use the right saddles to give you clearance from the wall. There will be enough space to get your grips, spanners etc around your workpiece and get it fitted. As long as the piece you're attaching to is securely fixed, you would be hard pushed to do any damage - it's steel!

     

    5. Lots of accessories, boxes, equipment etc can be connected to conduit systems, but don't worry if it's not obvious or straightforward at first. You can almost always adapt most things to suit, so don't be shy to make new holes or add conduit adaptors or the like.

     

    6. Experiment with it. There is no hard and fast rule to how you should install or use it. As long as the system is correctly supported throughout its length, and cable entries are protected with bushes/glands, design it how you see fit.

     

    And finally, wear gloves. Burrs and metal splinters in soft skin are no laughing matter! Use cutting compound for threads (if you don't already), and a good round or half round file is essential too.

     

    Hope this helps.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • chunkasmaximus
    0 chunkasmaximus over 5 years ago

    As with everything in life Rod H, practice makes perfect!

     

    Donald Lane's answer pretty much sums it up.

     

    You just have to work methodically and in one direction - don't try starting at two different points and meeting in the middle!

     

    I've not looked at what advice or videos are available, but as an electrician who has used the stuff on and off since college, the best advice I can sum up is the following (in no particular order):

     

    1. Practice and experiment joining different sections of conduit, boxes, accessories etc in small sections (using off cuts etc), then dismantle and reassemble. This will enable you to get used to doing things in the most efficient order. There's nothing worse than getting to a point, only to realise you have to undo it all. This will also help you with the planning of slightly larger scale installs, so you'll be less reliant on others for help.

     

    2. Use all the available fittings for your conduit system to make your life easier. Like already suggested in other comments, use fittings like running couplers, nipples, lock rings, bushes and the like. This will give you more flexibility and make assembly a little easier.

     

    3. Make the conduit bender your best buddy. A floor standing one is ideal, with a built-in vice if you can. It will be painful and it will take time but, the more you use it the less joints you'll have, the easier it will be to pull cables, and the neater it will look. It really is an art form, and if you plan to work with steel conduit long term, this is definitely a worthwhile investment.

     

    4. Use the right saddles to give you clearance from the wall. There will be enough space to get your grips, spanners etc around your workpiece and get it fitted. As long as the piece you're attaching to is securely fixed, you would be hard pushed to do any damage - it's steel!

     

    5. Lots of accessories, boxes, equipment etc can be connected to conduit systems, but don't worry if it's not obvious or straightforward at first. You can almost always adapt most things to suit, so don't be shy to make new holes or add conduit adaptors or the like.

     

    6. Experiment with it. There is no hard and fast rule to how you should install or use it. As long as the system is correctly supported throughout its length, and cable entries are protected with bushes/glands, design it how you see fit.

     

    And finally, wear gloves. Burrs and metal splinters in soft skin are no laughing matter! Use cutting compound for threads (if you don't already), and a good round or half round file is essential too.

     

    Hope this helps.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • 14rhb
    0 14rhb over 5 years ago in reply to chunkasmaximus

    Great advice, thank you chunkasmaximus ....and definitely the last point about gloves. When I get the bits I'll add in a few of these extra bushes, couplers, lock-nuts etc even if I'm nut sure where I intend to use them and them just experiment as you recommend.

     

    It also looks like you just joined Element14, so a warm welcome to you, and thanks again for jumping in with such helpful advice. Hopefully you'll enjoy the E14 community and take part in the projects, discussions, learning modules and roadtests image.

     

    Did you ever add a drain hole in the lower parts of an external installation incase water gets in ? What I find with anything sealed is that if it isn't perfect moist air gets drawn in and condenses but can never fully escape, instead it just builds up.

    • Cancel
    • Vote Up +3 Vote Down