Member's Forum Brewing beer - Automate the mashing process - where to start???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 632 subscribers
  • Views 1424 views
  • Users 0 members are here
  • help
  • rasberrypi
  • brewing
  • arduino
  • meshing
  • beginner
  • beer
Related

Brewing beer - Automate the mashing process - where to start???

e14 Contributor
e14 Contributor over 13 years ago

Hi Folks,

 

My name is Sebastian, I am from Berlin, Germany, I have a degree in computer science and recently started home brewing beer :-) . Since this is not only a lot of fun but also a lot of work I wanted to start automate part of the brewing process. I did some soldering when I was 10-12 but never got any "real" project done.

So basicly I don't have a clue yet where to start but I hope to get support from this great community and a push in the right direction. I think of using an Arduino or an RasberryPi plus some relays and temperature sensors...

 

So here is what I want to do:

 

When it comes to brewing beer you want to controll the temperature of the brewing kettle.

For example:

 

- 15 minutes at 55 degrees celsius.

- Then go up to 64 degrees celsius, holding it for 30 minutes,

- then  go up to 72 degrees celsius, holding it fo 20 minutes

- finally go up to 78 for 40 minutes.

 

There can be up to 5 steps which can be programmed by the user for each beer recipe. I think there is already some software out there which runs on the RasberryPI and I think this is where I will have the least problems. But I totally suck at soldering, knowing nothing about how to attach sensors (which sensors???) to the RasberryPi, what voltage to use etc etc.

So, I don't want to study for 2 years elecronics, but lets say a month. Where should I start? Are there some great beginners tutorials which you can recommend?

 

Thanks for every tip,

 

Cheers,

Sebastian

 

P.S. I have one of these, which I want to modify and then would be controlled by the Rasberry or Arduino: http://www.amazon.de/Weck-Einkochautomat-2000-Watt-Emaille/dp/B000PKEZL0/ref=sr_1_1?ie=UTF8&qid=1372698539&sr=8-1&keywords=einkochautomat+weck

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to PEarle

    Peter,

    - sounds like an excellent project for a Pi !

     

    Have you considered the RPi's MTBF rate when recommending

    it for process control applications such as home beer brewing?

    I've seen quite a few reports of RPi freezing, attributed to various factors

    such as X1 crystal stopping, USB packet dropping, SD card corruption,

    as well as unattributed causes.

     

    Some recent examples are mentioned on this thread:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=51&t=48383

     

    As you know, the RPi is intended more for teaching children to program,

    than for process control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • PEarle
    0 PEarle over 13 years ago

    Hi Sebastian - sounds like an excellent project for a Pi !

     

    This is a good article about using a temperature sensor with a Pi http://www.cl.cam.ac.uk/projects/raspberrypi/tutorials/temperature/.

     

    A lot of people start off with the Pi by making an LED flash on and off which is a good introduction to controlling circuits. You could have a look at this link https://projects.drogon.net/raspberry-pi/gpio-examples/tux-crossing/gpio-examples-1-a-single-led/. I used it as a guide when I did the same thing myself, which was my first attempt at electronics - I wrote a document about it which you can see here http://www.element14.com/community/docs/DOC-54238/l/blinking-an-led-with-the-piface.

     

    Best of luck !

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<