• Products and Partners
    Products and Partners
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
Member's Forum Anyone have an idea for a group project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 631 subscribers
  • Views 894 views
  • Users 0 members are here
Related

Anyone have an idea for a group project?

dwinhold
dwinhold over 13 years ago

I encourage anyone to submit ideas and as a group we can chose one to work on. When there are enough ideas we will have a poll for which one we do!!

  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 13 years ago

    Hi Dale,

     

    Ideas I have aplenty, but being disabled, making things has really slowed me down.

     

    I like the idea of a group project, so I will share some that I have.

     

    Project 1; A RC mobile magnetic ground mapper.  The Idea is to take an RC vehicle chassis and mount a metal detector so that the head of the detector can  be moved in an semi circle using a constant motion.  A MCU would then record the output readings every degree of arc and build up a map of the detections.  The RC vehicle would then advance an inch or two and the detector would swing through the arc again, building the next series of readings.

     

    The data could be off loaded for additional processing to make a full area map of the magnetic changes found when you cover an area.

     

    Goal, find buried metal such as land mines, coins, wire, cable, pipes, meteorites and other magnectic material.

     

    I can see a lot of applications for the RC vehicle in combing a large area for objects of interest in war zones and archeological sites.

     

    Thats all for now, but I will bring up other ideas as I have time.

     

    Enjoy,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dwinhold
    0 dwinhold over 13 years ago in reply to DAB

    Hello Dab,

     

    Your idea has really got me thinking. To go even a bit further I was thinking about having four detectors (each one 90deg from each other around the remote vehicle) that turn and scan like you suggest. This would give 360deg mapping, to add a bit we could connect to each detector head a sonar to map the ground at surface level. Gps would be a great addition so the user can pinpoint an exact position if needed. This type of vehicle would have many uses like you mentioned. I hope others will join in and add ideas or offer to help get this going. In most parts I probably have enough to get started on a project like this, but any help would be greatly accepted. From advice to programming, every bit helps. Lets try this out, I'm very interested.

     

    Thank you very much for the idea,

     

    Dale W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dwinhold
    0 dwinhold over 13 years ago in reply to DAB

    Hello Dab,

     

    Your idea has really got me thinking. To go even a bit further I was thinking about having four detectors (each one 90deg from each other around the remote vehicle) that turn and scan like you suggest. This would give 360deg mapping, to add a bit we could connect to each detector head a sonar to map the ground at surface level. Gps would be a great addition so the user can pinpoint an exact position if needed. This type of vehicle would have many uses like you mentioned. I hope others will join in and add ideas or offer to help get this going. In most parts I probably have enough to get started on a project like this, but any help would be greatly accepted. From advice to programming, every bit helps. Lets try this out, I'm very interested.

     

    Thank you very much for the idea,

     

    Dale W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 13 years ago in reply to dwinhold

    Hi Dale,

     

    I am glad you like the idea.

    I considered using multiple detectors and decided that you really only need one to get a full data set.

    Once you pass an area, you really do not need a double check if everything is working right.

    Plus, you keep the data rate down to a manageable level.  I am a firm believer in keeping the system simple.

    GPS would be a good addition, but I am not sure a sonic sensor would get you much useful data.

     

    In most cases, you want to map a given area in controlled search patterns.  That way you can cover the area with a good level of detail.

    Moving the detector in semicircles covers the area in front of and along the sides of the vehicle.  That way you do not drive over something you shouldn't.

    Moving in controlled steps lets you map the data over the surface with sufficient double checks with each pass to increase your detection probablility.

    Once you have enough samples, you can recalibrate the sample data to look for voids.  Voids can tell you if you have found a non-metallic object, such as a wood or plastic box buried in the area.  This approach is also useful in finding non-metallic land mines.  Also very useful to know.

     

    As for help, I would be glad to look over your design and data, but being disabled, I have a limited amount of capability to do more than that.

    Keep a running post going.  Who knows if you can pull in some additional helping hands/minds.

     

    I agree, it would be a very interesing device to tryout.  Just look at the guy in the UK who found 5 million pounds worth of gold viking artifacts.

    We know very little about what lurks beneath our feet.

     

    Good hunting,

    DAB